STEM Academy
  • Learn
  • Learning Center
  • STEM Academy
  • More
  • Cancel
STEM Academy
Blog TouchDevelop: A Killer Programming Language
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join STEM Academy to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 15 Jul 2015 9:44 PM Date Created
  • Views 3205 views
  • Likes 5 likes
  • Comments 13 comments
  • programming_languages
  • scratch
  • stem
  • python
  • microsoft
  • micro_bit
  • touch_develop
  • microbit
  • programing
  • arduino
  • touchdevelop
  • stem space
Related
Recommended

TouchDevelop: A Killer Programming Language

shabaz
shabaz
15 Jul 2015

Introduction

Up until yesterday, I’d not seen a programming language which would go from a graphic oriented (pseudo Scratch-like) environment to a conventional source code view, from browser based execution to microcontroller execution, to mobile phone app execution. It was possible however to achieve all of this within a matter of hours!

 

image

TouchDevelop is a programming language created by Microsoft – it can instantly run in a web browser if Internet connectivity is available, otherwise it can be locally installed too to run as a local web server. I tested a quick local install on Linux but of course it can be installed on Windows too.

 

TouchDevelop will be used with the micro:bit that Element14 and the BBC have developed together with Microsoft, ARM, Freescale and others as well as product champions including the IET and Cisco.

 

What can it do? How does it work?

Some key characteristics are:

• Browser based development environment (private server, or public cloud)

• Cloud storage of your programs

• Development environment optimised for touch interface for rapid copy/paste/delete and so on

• Forward/backward conversion between graphical block coding and text coding at any time

• Run anywhere - in a browser (i.e. any platform) or on hardware (microcontroller or mobile app for Android/IOS/Windows Phone)

• Will be supported for the micro:bit

• Open source – run local copies on any platform and OS (Linux, Windows, etc), and fork it and improve it!

 

This is how to use it to write code:

image

 

The nice thing is that programs can be developed anywhere and retained in a cloud provided you have a suitable account (based on delegated authentication so it doesn’t have to be a Microsoft account).

Although the install instructions were for Windows, it was relatively straightforward to install on Ubuntu and get coding.

Here is my attempt at turtle graphics:

image

 

There is also Arduino capability (see example code screenshot below) that can convert your program into C++ that can be used by the usual Arduino software tools – I didn’t get that compiling on Linux but I see no reason why this wouldn’t work with a little effort. The instructions for Windows are all published. With some more effort, other microcontroller platforms could in theory be supported since the output is standards based C++.

image

 

The screenshot above shows the blocks-based code view – clicking on the ‘plus’ symbol inserts a line. The syntax in blocks below changes dynamically as you create each row of the program.

Another option is to target your mobile device; if you have Android Studio and Apache Cordova installed then this is a quick affair (and I’ve never written a mobile app before) - here is the turtle program running on a Nexus device simulation:

image

 

As a personal opinion I think it is a far easier-to-use language than Scratch or Python, and the libraries and development environment are geared for modern scenarios where people want to be able to write code rapidly anywhere on any machine, even touch-based machines (e.g. iPads), and still have the flexibility to convert to the (relatively) low-level C++ so that native code can be built too, to run on as many different platforms as possible including resource-constrained ones such as Arduino.

 

Summary

The above was a very quick examination of TouchDevelop’s main features and what it could do. No real steps recorded since I was just exploring, but I think it is highly interesting and worthy of further investigation.

 

I think it is extremely powerful to have a single, simple language to learn for young and older people, and yet be able to target so many scenarios. The ability to write and access the code easily from any device is a significant advantage too.

 

A Getting Started guide will follow and will be indicated here so click on the Bookmark button if you’re interested to read it.

  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 11 years ago in reply to ntewinkel +3
    Hehe I noticed that, the tutorials point out exactly where to click, so it is impossible to code wrong! Very well implemented.
  • ntewinkel
    ntewinkel over 11 years ago in reply to mcb1 +2
    She's a really good web designer, and has fixed plenty of issues with WordPress (which is kind of like coding I suppose), but she's never done any application coding. Recently she's been designing the…
  • mcb1
    mcb1 over 11 years ago +1
    Nice ... 12blocks is a similar concept http://onerobot.org/products/12blocks/ Mark
Parents
  • mcb1
    mcb1 over 11 years ago

    Nice ...

     

    12blocks is a similar concept

    http://onerobot.org/products/12blocks/

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 11 years ago in reply to mcb1

    Hi Mark!

     

    Looks like the Scratch-like graphical programming environments are quite popular. 12blocks looks interesting according to that page, especially the graphing of variables for debugging, annotations with schematics and so on.

    I like that TouchDevelop is completely browser based though - opens up many opportunities, especially if kids have just a low-cost tablet or small iPod. I experimented a bit on my mobile, (the TouchDevelop environment presents a dedicated mobile view) and it was possible to tap out code and run it without having to bring up any keyboard overlay, which was very cool.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • shabaz
    shabaz over 11 years ago in reply to mcb1

    Hi Mark!

     

    Looks like the Scratch-like graphical programming environments are quite popular. 12blocks looks interesting according to that page, especially the graphing of variables for debugging, annotations with schematics and so on.

    I like that TouchDevelop is completely browser based though - opens up many opportunities, especially if kids have just a low-cost tablet or small iPod. I experimented a bit on my mobile, (the TouchDevelop environment presents a dedicated mobile view) and it was possible to tap out code and run it without having to bring up any keyboard overlay, which was very cool.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • mcb1
    mcb1 over 11 years ago in reply to shabaz

    I might have to look at it ..

    Not sure which Freedom boards to include in the suitcase ...

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 11 years ago in reply to mcb1

    Hehe I noticed my RIoTboard had been handled : )  (for some reason "someone" detached the jumper wires to a USB-to-serial board) with no note inside to state anything had been examined.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 11 years ago in reply to shabaz

    Interesting ...you should maybe ask why your bag was interferred with but no note left.

     

    Mark