CodeBug
  • Learn
  • Learning Center
  • STEM Academy
  • CodeBug
  • More
  • Cancel
CodeBug
Blog Blockly? Google? Google Blockly - wow!! How did I miss That!
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join CodeBug to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: e14 Contributor
  • Date Created: 18 Oct 2015 5:13 AM Date Created
  • Views 3845 views
  • Likes 6 likes
  • Comments 13 comments
Related
Recommended

Blockly? Google? Google Blockly - wow!! How did I miss That!

e14 Contributor
e14 Contributor
18 Oct 2015

I resigned myself to the task of finishing my next Codebug Blockly program yesterday and went in track of understanding better something that is either a bug or an as yet non utilized feature!! The right click menu for the Blockly blocks has a "help" option at the bottom for each block that opens another browser tab to a generic help guide on the Codebug website.. Trying to gather some extra info on the bug/feature that caused me nearly 2 hours worth of disabling, torture, disconnecting, anger, deleting, confusion, rebuilding, anguish and growling... lots and lots of GROWLING!!! GRRRrrrrrrRRRRR! - I randomly clicked on a block to get to the codebug help guide to try and sift through it for some clues and was surprised to be taken to the "Google Blockly" help guide?

 

I was like.."well it's very similar, and seems to have a more comprehensive instruction set - so what is it??"

 

It is Blockly. A Google product that can be configured and used by anybody for their own applications, it comes with a free Javascript, Python, <insert a few other scripting languages here>.

 

I went to the Blocky Editor there expecting it to be just as painful.. but wow!! There are more instructions, The drag and drop editor is responsive.. You know that lag that Codebug Blockly has?? The one that feels as if you are trying to drag virtual blocks through virtual treacle? Then have to sit and wait until the block you just dragged over snaps into place in case it doesn't want to and decides it wants to slip down and split up a very quick sum that took way too many more blocks than it should have and about 8 minutes and 22 seconds longer than it should have out of the 8 minutes and 24 seconds it took for the total construction of said sum? THEN THE DAMNED SCREEN SCROLLED TO THE BOTTOM AGAIN... AGAIN... AGAIN.... POX ON YOU!!

 

Have a quick try of the google editor interface... OK OK... Its still the same Blockly... I understand, I really do...

 

It's great for the novelty value, I know, its like when codeblocks and all the others appeared about 15 years ago when every compiler and target platform seemed to have it's own version... until they realised... programmers write programs, not stare blankly and hurt at a computer trying to fight off a weird boredom headache brought about by nonsensical, badly fitting, unimaginative, inefficient Jigsaws. Yep Jigsaws... and they didn't even bother to put pictures on the pieces... I found a Jigsaw today and realised it had never been out of the box.. In fact I can't recall a time that I did ever just sit there and do a jigsaw. There's a reason for that.. Jigsaws are for grannies. If you have a granny, give her the best gift She could get... Give her Blockly...

 

Sorry!! Just kind of went off on some random erm? thing. Hah!

 

Here's the link for the Blockly editor and other info about it in Googles product overview https://developers.google.com/blockly/ Really is so much zippier and reactive. As mentioned above, it comes with a Blockly to Javscript converter which explains why you can't edit the generated code on the codebug site.. the included compilers/converters only go one way... It also has an included Blockly to Python converter hmmmm? makes sense..

 

I'm determined to get this program finished!! The issue I had was solved but yeah... I totally need to de-stress my Blockly beans before I start rebuilding it all... 

  • Sign in to reply

Top Comments

  • e14 Contributor
    e14 Contributor over 10 years ago in reply to michaelkellett +2
    Hi Michael The idea was to try and come up with some fun alternative projects using the "out of the box" toolkit, kids really need a lot of motivation to get past the "new toy, I made the lights flash…
  • balearicdynamics
    balearicdynamics over 10 years ago in reply to e14 Contributor +2
    Why not interfere ? Interference and contamination is the core of the creativity
  • balearicdynamics
    balearicdynamics over 10 years ago in reply to shabaz +2
    Hi Shabaz, about the scrolling problem I have "discovered" (at the moment I have not yet read anywhere a decent documentation on all the - poor - editor features) that when you right-click on a object…
Parents
  • balearicdynamics
    balearicdynamics over 10 years ago

    Hey Lucie !

     

    that's all correct. Frankly as I saw the limits of the online programming system of the CodeBug - with some suspects in mind - I searched and found this Google project. That is open source. I don't remember where I read this sentence but if I am not totally wrong this is just the platform from where they started.

     

    I think it is not so difficult to manage the CodeBug with blocky, the only issue I see is the compilation process; as it is done by remote (veeeery bad) a CodeBug hack pass through the creation of a new, known bootloader. Then probably all the unused features of the PIC micro con be enabled on the device itself.

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • balearicdynamics
    balearicdynamics over 10 years ago

    Hey Lucie !

     

    that's all correct. Frankly as I saw the limits of the online programming system of the CodeBug - with some suspects in mind - I searched and found this Google project. That is open source. I don't remember where I read this sentence but if I am not totally wrong this is just the platform from where they started.

     

    I think it is not so difficult to manage the CodeBug with blocky, the only issue I see is the compilation process; as it is done by remote (veeeery bad) a CodeBug hack pass through the creation of a new, known bootloader. Then probably all the unused features of the PIC micro con be enabled on the device itself.

     

    Enrico