CodeBug
  • Learn
  • Learning Center
  • STEM Academy
  • CodeBug
  • More
  • Cancel
CodeBug
Blog CodeBug Project: Clock!
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join CodeBug to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 17 Oct 2015 10:48 PM Date Created
  • Views 1904 views
  • Likes 5 likes
  • Comments 3 comments
  • educational
  • clock
  • codebug
  • codebug_intermediate
Related
Recommended

CodeBug Project: Clock!

shabaz
shabaz
17 Oct 2015

With its 5x5 LED matrix, a binary coded decimal (BCD) clock is easy to create.

 

BCD is pretty easy - each column represents a digit, with the individual LEDs equating to 1, 2, 4 and 8.

If the first two LEDs in a column are lit then that means the digit is 3 (the sum of 1+2).

 

Here is a BCD example from wikipedia that represents the time 10:37 in BCD:

image

With the codebug I decided to build a 12-hour clock and to use the center LED to indicate the seconds:

image

 

When powered up, the default time is 1:00. To tweak the accuracy you may need to adjust the delay in the code.

To try it out or to modify and adapt to your taste,  click here for the BCD Clock.

Here is an example photo - excuse the quality!

image

  • Sign in to reply

Top Comments

  • mcb1
    mcb1 over 11 years ago +4
    knowing you that would be 0339 ... just when you finished playing with it. Well done. mark
  • jc2048
    jc2048 over 11 years ago +1
    That's nice - I like binary/BCD clocks. Have you thought of doing a stopwatch? Tens of seconds, seconds, tenths, and hundreths? One button to start the other to stop? Would be fun to play with. Could also…
  • shabaz
    shabaz over 11 years ago in reply to jc2048 +1
    Hi Jon, Interesting ideas! A stopwatch is a great idea. Speed measurement would be neat too. I need a few-minute timer for a coffee stove type thing, so connecting up a little buzzer to it would be cool…
Parents
  • mcb1
    mcb1 over 11 years ago

    knowing you that would be 0339 ... just when you finished playing with it.

     

     

    Well done.

    mark

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • mcb1
    mcb1 over 11 years ago

    knowing you that would be 0339 ... just when you finished playing with it.

     

     

    Well done.

    mark

    • Cancel
    • Vote Up +4 Vote Down