CodeBug
  • Learn
  • Learning Center
  • STEM Academy
  • CodeBug
  • More
  • Cancel
CodeBug
Blog CodeBug 'show n tell' - Spinny blocks
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join CodeBug to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: e14 Contributor
  • Date Created: 29 Sep 2015 3:59 AM Date Created
  • Views 4461 views
  • Likes 10 likes
  • Comments 31 comments
  • codebug
  • codebug_intermediate
Related
Recommended

CodeBug 'show n tell' - Spinny blocks

e14 Contributor
e14 Contributor
29 Sep 2015

Spinny Blocks

image

A CodeBug had made itself at home in my mail this morning; so I took the little guy in and decided to look after him!

 

Above is the CodeBug simulator showing a short sprite animation, you can see the animation running on a live CodeBug in the video below. All was done in the 'blocky' graphical code blocks editor which is intuitive to use and has the option of switching into a traditional text style editor.

 

I haven't tried the text editor yet, hopefully switching between the 2 will preserve true changes (graphical style editors have a habit of erasing or overwriting things entered manually).

 

I'm going to try using the iic and spi port soon but don't think those features have been enabled as yet, there is a download to allow it to act as a slave device but not in conjunction with the programs we can create, hopefully the firmware interpreter will mature overtime to allow things like this and also maybe inline asm or c for adding a bit of efficiency!

 

The mcu is a pic18f2550 and there are pogo pads for reprogramming the pic which opens up the option of using microchips C18 c compiler and programming your own firmware to it with an appropriate pickit programmer of some sort if the interpreter becomes too restrictive, however Im going to work as much with the installed interpreter, even considering trying to get a copy of the hex file so I can put it onto one of the 2550's in my dev box.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

  • Sign in to reply

Top Comments

  • e14 Contributor
    e14 Contributor over 11 years ago in reply to mcb1 +3
    Sometimes going back to basics and being restricted can lead to much more simple and fun things! and generate alternative solutions to problems! Remember that the led's are multiplexed and blinking on…
  • mcb1
    mcb1 over 11 years ago in reply to balearicdynamics +2
    It's a good challenge to do some IoT with these things Perhaps we should leave them as simple easy to program devices. I do wish there was an offline editor, and maybe it will come. Unfortunately the…
  • mcb1
    mcb1 over 11 years ago in reply to gregoryfenton +2
    The comment above disappeared ... I think Enrico has one arriving so problem solved. Mark
Parents
  • mcb1
    mcb1 over 11 years ago

    They are slightly adictive aren't they?

     

    Have you come up with a clever way to fasten to to clothes as a wearable.?

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to mcb1

    hi,

     

    I'm planning on keeping it intact with the firmware, not everybody has a pic programmer and it adds a layer of complexity that makes it less appealing.

     

    That doesnt mean that I arent going to try and push it beyond using the available commands in the graphics editor!

     

    This codebog maybe ending up in an enclosure like on the video but i do have a neat idea for attaching it to clothes, hopefully i'll come up with an example;

     

    lμcie

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to e14 Contributor

    Hi Lucie,

     

    I agree with you that making too complex hackings may result in a difficult approach especially by the main target of the kids this kind of device is created for. But I think that things should be saw by a slightly different point of view ... Let me check my unit as it arrives (UPS says tomorrow image ) and I can be more precise.

     

    Enrico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 11 years ago in reply to e14 Contributor

    not everybody has a pic programmer and it adds a layer of complexity that makes it less appealing

    Yes that is a good call.

     

    As much as the interface is clunky for those that can program, it does get someone interested in coding.

    I don't subscribe to scratch, and won't use it in our 'Arduino in Schools' program, but for this device and it's limited resources, it might be okay.

     

    I think I'll be trying to stick with using what is there and available on the board ...sure you will run out, but I've seen some amazing things from very little resource in the past.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • mcb1
    mcb1 over 11 years ago in reply to e14 Contributor

    not everybody has a pic programmer and it adds a layer of complexity that makes it less appealing

    Yes that is a good call.

     

    As much as the interface is clunky for those that can program, it does get someone interested in coding.

    I don't subscribe to scratch, and won't use it in our 'Arduino in Schools' program, but for this device and it's limited resources, it might be okay.

     

    I think I'll be trying to stick with using what is there and available on the board ...sure you will run out, but I've seen some amazing things from very little resource in the past.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to mcb1

    Sometimes going back to basics and being restricted can lead to much more simple and fun things! and generate alternative solutions to problems!

     

    Remember that the led's are multiplexed and blinking on and off really fast.

    • Cancel
    • Vote Up +3 Vote Down