CodeBug
  • Learn
  • Learning Center
  • STEM Academy
  • CodeBug
  • More
  • Cancel
CodeBug
Blog QuizBug, a CodeBug IoT educational project making-of
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join CodeBug to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: balearicdynamics
  • Date Created: 4 Oct 2015 12:38 PM Date Created
  • Views 4867 views
  • Likes 11 likes
  • Comments 25 comments
  • educational
  • codebug_sound
  • codebug
  • drobott_com
  • sound_effect
  • buzzer
  • codebug_advanced
  • drobott
  • quizbug
  • hardware_kit
  • iot
  • making_of
  • tindie
  • codebug_software
Related
Recommended

QuizBug, a CodeBug IoT educational project making-of

balearicdynamics
balearicdynamics
4 Oct 2015

A CodeBug Interactive Things project

 

Introduction

The first thoughts when the CodeBug board arrived on the market - and few time before reading the first reviews and technical tweets - was about how to create educational things (or, better, IoT) primarily targeted to newbies, joung enthusiasts, childs and students. The surrounding idea was to develop things moved by the CodeBug board. I mean objects for interaction, empowered by electronics involving making, programming, learning, hacking and customisation. This is how the idea of the CodeBug interactive things project was born.

image

The making-of shown below, the creation project to be clear, is the first one following in my opinion most of these line guides. I am almost against closed projects, especially if remaining open these can be source of inspiration to others.

So there is the product (and the assembly hacking kit) on the Drobott shop, and the self-hacking explanation in this article, with many thanks to the CodeBug provided by Element14 (if someone of you decides to buy one of them, don't forget to apply the Element14 discount code W0E49MYQ for a 10% off).

 

How it works

The proof of concept is almost simple: the CodeBug board controls a questions support board inclduing a 7x14 cm paper sheet. The sheet is expected showing a question with 5 possible options; one (or more) correct answers and the other wrong.

 

Thanks to the sensitive features of the CodeBug legs, no further accessory should be used: the user should touch with a finger the top-right conductive corner and one of the five possible answers with another. The answer response is shown on the CodeBug 5x5 LED display (a scrolling text) and the attached buzzer plays a wrong or correct sound effect.

 

Depending on how the back of the questions support board connectors are wired, it is possible configure one or more answers as correct and one or more answers as wrong, accordingly to the question image. The following image shows an example of single correct answer with three different types of questions.

image

Creating the Questions Support Board

The Questions Support Board Is machined with a 5 mm super-compact plastic foam creating the spaces for the question paper sheet and the conductive areas. The conductive areas are obtained by adhesive soldering copper belts 2 cm wide; the front area (visible) of the copper is used to "touch" the answers while the back side of the belt (hidden to the user) are wired together depending on the kind of options that should be correct and wrong.image

 

The images below shows the assembly phase of a question support board with contacts and back soldered wires.

imageimage

imageimage

The resulting board has a size of 10x15 cm with a question image area of 7x14 cm.

image

Connecting to the CodeBug

When the boards are created the first three top-left contacts should be legged to the CodeBug respectively from left to the right with Leg 1, GND and Leg 3, accordingly with the program that responds with a correct answer on Leg 1 and wrong answer on Leg 3.

image

For a more impacting effect when the user touch on of the answers some sound effects has been generated bit-banging a buzzer (or a very small speaker). In this case the 5V leg of the CodeBug should be connected to the positive wire of the buzzer while the negative is connected to the Leg 0.

image

The following video shows the QuizBug at work.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

The software

The QuizBug software can be remixed on the CodeBug site and modified as well or used as-is. The commented images below analyses in detail the different blocks of code.

image

Most of the variable used in the program are declared on top. This makes a simple job any further change for a different reactivity or behavior of the program without the need to change the instructions. The variable ResponseString is defined initially with a dummy content (it is never used) to optimize the response speed; only the variable content is changed instead of using two different sprites.

Changing the values of low and speed different sound effects can be generated by the buzzer.

 

The program wait until a button (A or B) is pressed then after the variables definition starts an infinite loop. The different activities are controlled by flags that decides what conditions are verified according with the user interaction.

image

Every time the user press the button A the OnOffStatus changes. When it is true, a new answer can be tried else the program waits until the user does not start it.

image

Thanks to set the variables of the program on top, when the leg status (corresponding to the answer) is checked, only some flags and variables should be changed; Accordingly with the leg the ResponseString content is set to correct or wrong (instead of designing two different sprites). The value of Raise (+1 or -1) is set to change the direction of the sound effect, growing for the correct answer and falling for the wrong answer. The flag AnswerStatus is normally set to false when the program is waiting for the user interactions. When a choice is detected, it is set to true for the answer response animation.

image

If AnswerStatus is true, the user has pressed one of the possible answers and two separate events are executed in sequence: the sound effect generation and the scrolling text with the answer response. As the variables has already been set before, only one action should be executed valid for both the conditions of the program.

Attachments:
imageQuestionary-Template A4.pdf
  • Sign in to reply

Top Comments

  • DAB
    DAB over 11 years ago +2
    Nice project. It is amazing what you can do with simple devices and a little imagination. DAB
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to balearicdynamics +2
    I agree, I would definitely like to see the memory/codespace usage! Im away from home for a few days tomorrow but when I get back Im going to look into the python interface. It offers a little more control…
  • mcb1
    mcb1 over 11 years ago +2
    Nice work. When you first suggested it, I was a little puzzled how it would turn out. This is very clever and has some interesting options. Mark
Parents
  • spannerspencer
    spannerspencer over 11 years ago

    Nice work, man! Great design. It'd be cool to compile these into a kind of book, with the CodeBug attached.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to spannerspencer

    Hey Spanner! Thank you.

     

    You always relaunch ideas ... Nice image Please, explain what do you mean (maybe some neural process in our two brain overlap image)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • spannerspencer
    spannerspencer over 11 years ago in reply to balearicdynamics

    Well, each of the boards kind of reminds me of a children's book (the kind with big chunky pages, that often have lots of different textures and such, if you know what I mean?). If they could be connected together down the left hand side with some kind of spine, kids (or anyone, really!) could play the current board, flip the page and play all the way through the "book" image

     

    I guess it'd need some kind of clever contacts mechanism to connect each "page" to the CodeBug as you turn it over, though...

     

    And maybe the CodeBug could be built into the cover of the book, so all that's showing is the display?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to spannerspencer

    Yes there was coincidence. ...

     

    I though to this, but I should find a market to place the book. This as-is is a kid / non kid game, while when finally assembled is the final stable version. I really should find a "somewhere" to sell some of these. Also my wife that is a translator immediately saw this as a great tool for small child language teaching. Nice and enjoying. And it is not difficult to make in practice. Every "page" will have two small holes outside, for the two rings. Up to 10 pages can fit (= 5 cm thick). Cover will be the same with the CB on the cover making the display.

    And in the meantime the joke can be reprogrammed, changed, changing sounds etc.

     

    I think I will continue with the series, I should admit that in a couple of days seeing just the tweets it was a discrete success.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • spannerspencer
    spannerspencer over 11 years ago in reply to balearicdynamics

    Somewhere like Etsy might be a good marketplace for this?

     

    One final thought, just to overcomplicate things image

     

    I wonder if it'd be possible to create a kind of "blank" book, with just the pages (say, five or six), and you slide in the pictures. These could be thin, laminated pictures, with flexible tracks on the back to replace the ribbon cable you used in the prototype. That way, someone could buy the blank book, and then purchase new "themes/stories/games" just as a pack of replacement pictures. Could be a good way to keep people buying new "books" cheaply, but more often image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • spannerspencer
    spannerspencer over 11 years ago in reply to balearicdynamics

    Somewhere like Etsy might be a good marketplace for this?

     

    One final thought, just to overcomplicate things image

     

    I wonder if it'd be possible to create a kind of "blank" book, with just the pages (say, five or six), and you slide in the pictures. These could be thin, laminated pictures, with flexible tracks on the back to replace the ribbon cable you used in the prototype. That way, someone could buy the blank book, and then purchase new "themes/stories/games" just as a pack of replacement pictures. Could be a good way to keep people buying new "books" cheaply, but more often image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to spannerspencer

    If you take a look to the Drobott.com store I have already put the "product" in different versions, i.e. the add-on pack. This is for DIY the book, hack, modify etc. and is viewed under the concept of "kit". As you can see in the post there is a PDF template attached to create the different sheets. As I told, this is in the logic of the DIY QuizBug kit. The same kit is already on Tindie market.

     

    Then the idea of the book can be just for Etsy, the excellence market of the good handcrafted things. There there is no space for bare electronics but maybe space for these kind of stuff. Not only, but we (my wife and me) are also registered editors, publishing on ebook and paperback format almost regularly (Amazon.com: ediciones baleares ) and we can also publish this as a child book (with a series of different sheets as you mentioned, that are the same I shown in the prototype on the post) In this case I see two order of blocking problems: first we should include (mandator IMO) the codebug inside its cover with design etc. And this is NOT an open source device, so it is not possible also for legal questions to sell as part of another product. If you already have, you can buy the kit as the tons of accessories of the Raspberry PI.

    The second most important and (sic!) blocking thing is that to make just 10 units to make a stupid test on the market - also with the luck that all will be sold in few time, that is not so obvious - means an investment of at least 150Euro in CodeBug devices (that we can't include for the reasons above) plus the machined material that needs time, and this plastic that is atossic, compact but with a good perception, quality etc. has a cost too.

     

    Obviously this idea is great if you think that maybe a series (there are the others, the cube with insets, the car race, the micro train etc.) where Dad or bigger borther or sister plays and makes always new games to the childs...

     

    Suggestions ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • spannerspencer
    spannerspencer over 11 years ago in reply to balearicdynamics

    Certainly it's no small investment, as you say, and I'm not too sure about the legalities of including a CodeBug in the package (which seems like something of a necessity). But for someone with more of a business and manufacturing mind than I have, it still seems like a solid idea image

     

    I'm quite keen to see the racing car idea next image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to spannerspencer

    About the investment it's anyway possible, maybe if some kit is sold, if if if ... But maybe. Instead I am 99% sure that it is not possible to include a CodeBug inside the package. By this side the only thing I see is just to leave the hole where the use put the CB inside. Something like a veeeery special case image

     

    We'll see the next idea. Then see what happens. image