CodeBug
  • Learn
  • Learning Center
  • STEM Academy
  • CodeBug
  • More
  • Cancel
CodeBug
Blog QuizBug, a CodeBug IoT educational project making-of
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join CodeBug to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: balearicdynamics
  • Date Created: 4 Oct 2015 12:38 PM Date Created
  • Views 4937 views
  • Likes 11 likes
  • Comments 25 comments
  • educational
  • codebug_sound
  • codebug
  • drobott_com
  • sound_effect
  • buzzer
  • codebug_advanced
  • drobott
  • quizbug
  • hardware_kit
  • iot
  • making_of
  • tindie
  • codebug_software
Related
Recommended

QuizBug, a CodeBug IoT educational project making-of

balearicdynamics
balearicdynamics
4 Oct 2015

A CodeBug Interactive Things project

 

Introduction

The first thoughts when the CodeBug board arrived on the market - and few time before reading the first reviews and technical tweets - was about how to create educational things (or, better, IoT) primarily targeted to newbies, joung enthusiasts, childs and students. The surrounding idea was to develop things moved by the CodeBug board. I mean objects for interaction, empowered by electronics involving making, programming, learning, hacking and customisation. This is how the idea of the CodeBug interactive things project was born.

image

The making-of shown below, the creation project to be clear, is the first one following in my opinion most of these line guides. I am almost against closed projects, especially if remaining open these can be source of inspiration to others.

So there is the product (and the assembly hacking kit) on the Drobott shop, and the self-hacking explanation in this article, with many thanks to the CodeBug provided by Element14 (if someone of you decides to buy one of them, don't forget to apply the Element14 discount code W0E49MYQ for a 10% off).

 

How it works

The proof of concept is almost simple: the CodeBug board controls a questions support board inclduing a 7x14 cm paper sheet. The sheet is expected showing a question with 5 possible options; one (or more) correct answers and the other wrong.

 

Thanks to the sensitive features of the CodeBug legs, no further accessory should be used: the user should touch with a finger the top-right conductive corner and one of the five possible answers with another. The answer response is shown on the CodeBug 5x5 LED display (a scrolling text) and the attached buzzer plays a wrong or correct sound effect.

 

Depending on how the back of the questions support board connectors are wired, it is possible configure one or more answers as correct and one or more answers as wrong, accordingly to the question image. The following image shows an example of single correct answer with three different types of questions.

image

Creating the Questions Support Board

The Questions Support Board Is machined with a 5 mm super-compact plastic foam creating the spaces for the question paper sheet and the conductive areas. The conductive areas are obtained by adhesive soldering copper belts 2 cm wide; the front area (visible) of the copper is used to "touch" the answers while the back side of the belt (hidden to the user) are wired together depending on the kind of options that should be correct and wrong.image

 

The images below shows the assembly phase of a question support board with contacts and back soldered wires.

imageimage

imageimage

The resulting board has a size of 10x15 cm with a question image area of 7x14 cm.

image

Connecting to the CodeBug

When the boards are created the first three top-left contacts should be legged to the CodeBug respectively from left to the right with Leg 1, GND and Leg 3, accordingly with the program that responds with a correct answer on Leg 1 and wrong answer on Leg 3.

image

For a more impacting effect when the user touch on of the answers some sound effects has been generated bit-banging a buzzer (or a very small speaker). In this case the 5V leg of the CodeBug should be connected to the positive wire of the buzzer while the negative is connected to the Leg 0.

image

The following video shows the QuizBug at work.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

The software

The QuizBug software can be remixed on the CodeBug site and modified as well or used as-is. The commented images below analyses in detail the different blocks of code.

image

Most of the variable used in the program are declared on top. This makes a simple job any further change for a different reactivity or behavior of the program without the need to change the instructions. The variable ResponseString is defined initially with a dummy content (it is never used) to optimize the response speed; only the variable content is changed instead of using two different sprites.

Changing the values of low and speed different sound effects can be generated by the buzzer.

 

The program wait until a button (A or B) is pressed then after the variables definition starts an infinite loop. The different activities are controlled by flags that decides what conditions are verified according with the user interaction.

image

Every time the user press the button A the OnOffStatus changes. When it is true, a new answer can be tried else the program waits until the user does not start it.

image

Thanks to set the variables of the program on top, when the leg status (corresponding to the answer) is checked, only some flags and variables should be changed; Accordingly with the leg the ResponseString content is set to correct or wrong (instead of designing two different sprites). The value of Raise (+1 or -1) is set to change the direction of the sound effect, growing for the correct answer and falling for the wrong answer. The flag AnswerStatus is normally set to false when the program is waiting for the user interactions. When a choice is detected, it is set to true for the answer response animation.

image

If AnswerStatus is true, the user has pressed one of the possible answers and two separate events are executed in sequence: the sound effect generation and the scrolling text with the answer response. As the variables has already been set before, only one action should be executed valid for both the conditions of the program.

Attachments:
imageQuestionary-Template A4.pdf
  • Sign in to reply

Top Comments

  • DAB
    DAB over 11 years ago +2
    Nice project. It is amazing what you can do with simple devices and a little imagination. DAB
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to balearicdynamics +2
    I agree, I would definitely like to see the memory/codespace usage! Im away from home for a few days tomorrow but when I get back Im going to look into the python interface. It offers a little more control…
  • mcb1
    mcb1 over 11 years ago +2
    Nice work. When you first suggested it, I was a little puzzled how it would turn out. This is very clever and has some interesting options. Mark
Parents
  • e14 Contributor
    e14 Contributor over 11 years ago

    Hey Enrico!

     

    This is a superb addition to Codebug examples!

     

    How are you finding working with blockly gui? i find it really difficult, its just not fast enough if you understand what i mean (not to mention the way the screen constantly scrolls to the bottom). Im wondering if its responsive enough to keep the attention of kids?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to e14 Contributor

    Hey Lucie image

     

    The program is responsive as I have optimised it as much as possible (also the most important optimisation is mentioned. It is responsive and I was surprised how fast is this stuff ... Take a look to the video, also while completing an answer (no need pen, contact etc.: just only the hands that is perfect for young children.

     

    First the problem of the grpahic guy has an incredible limitation, no sub-block calling so it's a incredible exercise to make the code working with multiple conditions. The better solution is using if conditions where the longest process is never the default condition so the program can loop fine. The other problem is the impossibility to use interrupts so you should continuously test a good balance between the events and their duration to avoid annoying bottlenecks in the execution impacting on bad efficient usability.

     

    Then ... yes, the graphic guy is really a mess. Bad Web interface and bad blocks management. The main problems I have found are

    • Too slow editing.
    • Non efficient programs when the code comes consistent, more than a simple single event.
    • Excluding the Remix function it is impossible to copy and paste the code between different applications
    • Block editing is too small
    • Block paste function with long applications is a mess to move in another place of the program
    • Impossible to save locally the code, so as a matter of fact code is only saved on their server. This makes the creations too fragile. I should find a hack at least to make backups.

     

    Then... a lot of other wrong stuff (including the remote compiling).

     

    Ah - forgot - when the program comes a minimum consistent, the remote compilation is far to be fast image And there is no option to know before what is the memory space user, program space etc. Very bad software approach also for child IMHO.

     

    Happy that you liked this first thing. There are other coming soon image

     

    Cheers. Enrico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to e14 Contributor

    Hey Lucie image

     

    The program is responsive as I have optimised it as much as possible (also the most important optimisation is mentioned. It is responsive and I was surprised how fast is this stuff ... Take a look to the video, also while completing an answer (no need pen, contact etc.: just only the hands that is perfect for young children.

     

    First the problem of the grpahic guy has an incredible limitation, no sub-block calling so it's a incredible exercise to make the code working with multiple conditions. The better solution is using if conditions where the longest process is never the default condition so the program can loop fine. The other problem is the impossibility to use interrupts so you should continuously test a good balance between the events and their duration to avoid annoying bottlenecks in the execution impacting on bad efficient usability.

     

    Then ... yes, the graphic guy is really a mess. Bad Web interface and bad blocks management. The main problems I have found are

    • Too slow editing.
    • Non efficient programs when the code comes consistent, more than a simple single event.
    • Excluding the Remix function it is impossible to copy and paste the code between different applications
    • Block editing is too small
    • Block paste function with long applications is a mess to move in another place of the program
    • Impossible to save locally the code, so as a matter of fact code is only saved on their server. This makes the creations too fragile. I should find a hack at least to make backups.

     

    Then... a lot of other wrong stuff (including the remote compiling).

     

    Ah - forgot - when the program comes a minimum consistent, the remote compilation is far to be fast image And there is no option to know before what is the memory space user, program space etc. Very bad software approach also for child IMHO.

     

    Happy that you liked this first thing. There are other coming soon image

     

    Cheers. Enrico