STEM Academy
  • Learn
  • Learning Center
  • STEM Academy
  • More
  • Cancel
STEM Academy
Forum Wind turbine design
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join STEM Academy to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 18 replies
  • Subscribers 59 subscribers
  • Views 4236 views
  • Users 0 members are here
  • stem space
Related

Wind turbine design

e14 Contributor
e14 Contributor over 11 years ago

OK not sure whether this should be here or in power management, but I am choosing engineering

 

This is a new subject to me in relation to the physical build of a turbine

 

I wonder if anyone can tell me why the vanes are perpendicular to the wind direction instead of parallel to the flow of wind

 

In my eyes it may be easier to build a turbine with variable direction blades depending on the speed of the wind so that they are facing the sky, which would reduce the directional workings from the complexity of the design

  • Sign in to reply
  • Cancel

Top Replies

  • dragonstyne
    dragonstyne over 11 years ago in reply to mcb1 +1
    I agree, over reving is a big issue also, more surface area provides better performance in lower wind situations. Larger wind turbines tend to create RF noise due the varying capacitance between the blades…
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to dragonstyne +1
    Are now we are getting into different area of problems that I had forgotten about EMF and RF interference, I remember testing equipment against that (in an old employment) but had not even thought about…
Parents
  • amgalbu
    amgalbu over 11 years ago

    The main reason for the configuration you see in windmill is efficienc. That's the same reason why you don't see anymore the steamboats with the two big wheels: a propropeller is more efficient

    I don't what your aims are, but you could also have a look at windbelts

     

    http://www.tomsguide.com/us/wind-power-ene…

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • amgalbu
    amgalbu over 11 years ago

    The main reason for the configuration you see in windmill is efficienc. That's the same reason why you don't see anymore the steamboats with the two big wheels: a propropeller is more efficient

    I don't what your aims are, but you could also have a look at windbelts

     

    http://www.tomsguide.com/us/wind-power-ene…

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to amgalbu

    Thanks I will have to look into this in more detail

     

    Ok - had a look at this; it is on the principle of an electric guitar string, producing any real power from this looks very limited, but I might be wrong, an in depth look at technology of magnetic and piezo picks would have to be done