STEM Academy
  • Learn
  • Learning Center
  • STEM Academy
  • More
  • Cancel
STEM Academy
Forum I need advice on a project.
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join STEM Academy to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 4 replies
  • Answers 1 answer
  • Subscribers 54 subscribers
  • Views 1345 views
  • Users 0 members are here
  • detectors
  • light_detectors
  • stem space
Related

I need advice on a project.

mikedavis
mikedavis over 13 years ago

Everyone,

 

I have an idea for a project, and I need some assistance. 

 

I would like to use the RPi (or whatever is most appropriate) to create a light detector.

 

A long time ago, I built a circuit that had a cadmium selenide detector.  When light hit it, there was a change in its resistance, and I could use the difference between the voltage in and the voltage out to determine how much light the detector was seeing.

 

I have breadboard that I can use to get the circuit going.  I would like to be able to use the RPi to have a computer capture this information so I could run an experiment over a long period of time.

 

What materials would I need?

 

Mike Davis

  • Sign in to reply
  • Cancel

Top Replies

  • DAB
    DAB over 13 years ago +1 suggested
    Hi Mike, The selection of a MCU will depend upon the details of your long term project. Have you assessed if the sensor can cover the light lntensity levels you need? How ofter do you plan to sample the…
  • bltsandwich1
    bltsandwich1 over 13 years ago +1
    The Arduino is a great tool, and it can be used very easily with sensors such as a light sensor that you mention. The real challenge is going to be whether or not you are able to get the output you really…
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Mike, a couple of suggestions:

     

    Keep your circuit mostly as-is and use an I2C (or SPI) ADC chip to read the change in the LDR in place of a simple analogue meter. There are plenty of ADC's available with different resolutions and sampling speeds, perhaps something like this ADC081C027CIMK/NOPB - IC, 8BIT ADC, I2C, SAR, TSOT23-6ADC081C027CIMK/NOPB - IC, 8BIT ADC, I2C, SAR, TSOT23-6

     

    Another way might be to use a specific light sensor like TSL2550DTSL2550D   

     

    Either way, and as DAB suggests, you'll need to make sure the device you chose has the required sensitivity.

     

    Both of those suggestions could be interfaced directly to an RPi, or to an Arduino. Reading them at set intervals and writing the results to somewhere useful is simply a matter of writing some code to do it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Mike, a couple of suggestions:

     

    Keep your circuit mostly as-is and use an I2C (or SPI) ADC chip to read the change in the LDR in place of a simple analogue meter. There are plenty of ADC's available with different resolutions and sampling speeds, perhaps something like this ADC081C027CIMK/NOPB - IC, 8BIT ADC, I2C, SAR, TSOT23-6ADC081C027CIMK/NOPB - IC, 8BIT ADC, I2C, SAR, TSOT23-6

     

    Another way might be to use a specific light sensor like TSL2550DTSL2550D   

     

    Either way, and as DAB suggests, you'll need to make sure the device you chose has the required sensitivity.

     

    Both of those suggestions could be interfaced directly to an RPi, or to an Arduino. Reading them at set intervals and writing the results to somewhere useful is simply a matter of writing some code to do it.