STEM Academy
  • Learn
  • Learning Center
  • STEM Academy
  • More
  • Cancel
STEM Academy
Forum Project Ideas Needed: Environmental Science with Arduino or Raspberry Pi
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join STEM Academy to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 15 replies
  • Answers 1 answer
  • Subscribers 58 subscribers
  • Views 7441 views
  • Users 0 members are here
  • sensing
  • raspberry
  • environment
  • oceanography
  • science
  • weather
  • aquarium
  • arduino
  • stem space
Related

Project Ideas Needed: Environmental Science with Arduino or Raspberry Pi

e14 Contributor
e14 Contributor over 12 years ago

I'm looking for ideas/projects we can design using an Arduino or Raspberry Pi with high school students. My students are participating in Make/Google's Summer Maker Camp and they just sent us a couple of Arduino Unos to build our projects around. Since I'm really new to single-board computers, I'd love to hear from everyone here for ideas..

 

It would be awesome if we could find projects related to:

  • Environmental Science (like the one mentioned in this post)
  • Oceanography
  • Animal Health

We just ordered a couple copies of this book about Environmental Sensing and Ardiuno from MakerShed.com.

image

We think these devices would be great for sensing things in the environment (such as temperature, pressure, water quality, etc.), but we are also looking for ways to output that data.

 

If anyone has links, suggestions or even just wants to brainstorm ideas for how an Arduino or Raspberry Pi might be used at an aquarium (I work at Shedd Aquarium in Chicago), then let me know!

 

 

 

 

Re: Ideas for using the Raspberry Pi in the classroom

  • Sign in to reply
  • Cancel

Top Replies

  • mikedavis
    mikedavis over 12 years ago +1 suggested
    Hey Wade. I am Mike Davis, and I work with the City Colleges of Chicago. I think you guys have a golden opportunity to do some fun things. One thing I'd recommend is making use of gspread. It is something…
  • gadget.iom
    gadget.iom over 11 years ago in reply to nbizzell +1
    That's an awesome project! Hamsters can cover some milage.
  • DAB
    DAB over 11 years ago +1
    One of the best ways to begin looking at issues in the environment is to measure and record the parameters in your local area. The Arduino provides a great way to set up sensors for data logging over a…
Parents
  • mikedavis
    0 mikedavis over 12 years ago

    Hey Wade.  I am Mike Davis, and I work with the City Colleges of Chicago.  I think you guys have a golden opportunity to do some fun things.

     

    One thing I'd recommend is making use of gspread.  It is something that collects information from a sensor and throws it right into a Google Spreadsheet.  I've been using a Raspberry Pi and a temperature probe for some simple cooling curves.  I think it is perfect for the kind of thing where you can track things like temperature, pressure, CO2, etc over long periods of time.  The next step would be to make a GUI for it, and maybe a dashboard.

     

    This site is a good guide, but you will have to modify some things.  I will be posting instructions soon.

     

    Using sensors you might be able to capture something with your phosphorescent fish.  A Cadmium selenide sensor can be used to detect light.  I think there would be something really interesting there.

     

    Here is something with a boat.

     

    http://www.raspberrypi.org/fish-pi/

     

    You could probably do something with a waterproof camera and a sensor.  Every time something touches it, it would tweet a photo.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • mikedavis
    0 mikedavis over 12 years ago

    Hey Wade.  I am Mike Davis, and I work with the City Colleges of Chicago.  I think you guys have a golden opportunity to do some fun things.

     

    One thing I'd recommend is making use of gspread.  It is something that collects information from a sensor and throws it right into a Google Spreadsheet.  I've been using a Raspberry Pi and a temperature probe for some simple cooling curves.  I think it is perfect for the kind of thing where you can track things like temperature, pressure, CO2, etc over long periods of time.  The next step would be to make a GUI for it, and maybe a dashboard.

     

    This site is a good guide, but you will have to modify some things.  I will be posting instructions soon.

     

    Using sensors you might be able to capture something with your phosphorescent fish.  A Cadmium selenide sensor can be used to detect light.  I think there would be something really interesting there.

     

    Here is something with a boat.

     

    http://www.raspberrypi.org/fish-pi/

     

    You could probably do something with a waterproof camera and a sensor.  Every time something touches it, it would tweet a photo.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to mikedavis

    Great to virtually meet you Mike! Thanks for the awesome collection of information. gspread sounds like a great place to start, and we just got the ebooks I mentioned in my previous post which talk about projects and types of data to collect.

     

    Your idea with the waterproof camera, sensor and tweet also sounds very interesting. It reminds me of a project being run in Australia to publicly share shark locations via twitter (obviously at a larger scale).

     

    I need to step my skills up (I'm a beginner with Arduinos and Raspberry Pis), so I'm going to work with our teens to create the projects from Make/Google's summer camp. I'll share those here, and then I'll be back with more questions about some of the projects you mentioned.