STEM Academy
  • Learn
  • Learning Center
  • STEM Academy
  • More
  • Cancel
STEM Academy
Forum Getting Started on a Breadboard
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join STEM Academy to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 19 replies
  • Subscribers 60 subscribers
  • Views 7576 views
  • Users 0 members are here
  • circuits
  • stem
  • breadboards
  • tlcfeedback
  • theheckwithkaren
  • learning
  • theheckwkaren
  • beginner
Related

Getting Started on a Breadboard

makerkaren
makerkaren over 8 years ago

I run workshops to teach STEM basics, sometimes to adults, often to children. Soldering is not always an option, so I've been trying to come up with simple projects to build on a breadboard with fairly inexpensive parts, to show how to make a circuit that does something visually obvious, such as turn on a motor or lights. The groups that organize these workshops frequently have very low budgets to where they couldn't afford enough Arduino or Raspberry Pis or the like for the entire group. I'm frequently given a $50-100 budget for anywhere between 6 and 30 individuals. What fun projects could be built on breadboards that are simple enough for a child to be able to understand? I've found that the best received projects are ones with a result that is the kids can see; a light turns on, a motor spins, etc.

One of the goals of these projects would be reusing the parts for other projects or with another group, so nothing with the project should be destructive.

What simple circuits helped you to learn electronics?

image

  • Sign in to reply
  • Cancel

Top Replies

  • DAB
    DAB over 8 years ago +5
    Hi Karen, I would start with the venerable 555 timer chip. It would let you explore both analog and digital circuits so you can start with simple logic, clocks, PWM, and then look at analog issues like…
  • fmilburn
    fmilburn over 8 years ago +3
    Hi Karen, There are lots of simple circuits to blink, buzz, move and even sense on a breadboard as you point out. I think the key with kids is to get results quickly, at least at first, and tie it to something…
  • gam3t3ch
    gam3t3ch over 8 years ago +3
    For me starting with a 555 timer helped me the most back in the day I enjoyed making projects and trying new things with the 555 timer, this brought me into other projects with IR as well for projects…
Parents
  • e14phil
    e14phil over 8 years ago

    I highly recommend a few SUPER simple, Super quick exercises just to to stress how the electrons flow and the how the power rails work.

     

    1) Draw a circular circuit of  Battery > Resistor > LED.

    2) Show them what direction the sockets are connected

    3) Show them the Power Rails

    4) Wire the Battery > Resistor > LED on the breadboard, stressing the flow of the circuit.

    5) Add the complexity of a push button / switch to the diagram and then to the circuit

     

    I know its super over kill simple, but it took seeing it in that order for me to put aside my apprehension/prejudices about breadboards being "complex and scary" when I first started.

     

    Phil

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • makerkaren
    makerkaren over 8 years ago in reply to e14phil

    That's a really good point. Learning electronics has been a constant struggle for me. Learning to read a diagram and knowing how to make that translate into parts on a breadboard really connects the dots. As someone that tends to learn quickly, I've tried starting with more complex circuits and projects and struggled to really understand how they work. I could make them work, but didn't understand what was happening within the circuit. Sometimes starting at the very basics is what is needed to create a solid foundation for more advanced learning later. Thanks!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • makerkaren
    makerkaren over 8 years ago in reply to e14phil

    That's a really good point. Learning electronics has been a constant struggle for me. Learning to read a diagram and knowing how to make that translate into parts on a breadboard really connects the dots. As someone that tends to learn quickly, I've tried starting with more complex circuits and projects and struggled to really understand how they work. I could make them work, but didn't understand what was happening within the circuit. Sometimes starting at the very basics is what is needed to create a solid foundation for more advanced learning later. Thanks!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Children
  • DAB
    DAB over 8 years ago in reply to makerkaren

    Back in Tech School (1970), they started with Ohms law and had us play with resistors and DC voltages.

    Then we moved on to capacitors, inductors and AC voltage.

    We then worked up to using tubes to build circuits.

     

    At every step, we worked with simple circuit designs to get everyone familiar with circuit layout and how to trace the circuit from input to output.

     

    It takes a while to make this process intuitive.  Persistence is required.

     

    Keep at it until it becomes second nature.

     

    DAB

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • luislabmo
    luislabmo over 8 years ago in reply to makerkaren

    I think e14phil's list is on spot, I could add few more which can come after his list and are very easy on the budget.

    • Explain how a switch works (battery + resistor + led + switch), here you can explain with push buttons Normally Open/Close and maybe add examples with a slide switch.
    • Ohm's law: using different resistor's values changes the led brightness (battery + various resistors + led)
    • Dimmer (variable resistors): (battery + potentiometer + led + switch). Here they can learn how a Potentiometer works.
    • Demonstrate how capacitors work -Charge/Discharge- (battery + electrolytic capacitor + resistor + led)

     

    Moving to some more complex, transistors / 555 can be added to the mix and they all re-use previous concepts learned (capacitors, ohm's law, switches, variable resistors)

    • Blinking led's
    • Dimmer
    • Police siren

    I know micro-controllers can be too advanced, but if you ever get there, all examples above can be done easily with very few lines of code using an arduino or ATtiny micro-controller. Very good example here.

     

    Luis

    • Cancel
    • Vote Up +3 Vote Down