microbit
  • Learn
  • Learning Center
  • STEM Academy
  • microbit
  • More
  • Cancel
microbit
micro:bit Blog BBC micro:bit - Submit your Big Ideas
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join microbit to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jlucas
  • Date Created: 14 Jun 2016 4:23 PM Date Created
  • Views 7550 views
  • Likes 13 likes
  • Comments 47 comments
  • bit
  • micro:bit
  • bbc micro:bit
  • bbc
  • microbit
  • big ideas
  • ten bbc micro:bit projects
Related
Recommended

BBC micro:bit - Submit your Big Ideas

jlucas
jlucas
14 Jun 2016

image

 

Introduction

 

Our 10 BBC micro:bit Projects in 10 Days series introduced the incredible creative potential of this unique pocket sized computer system. But we've really only scratched the surface. Now we want to hear your ideas.

 

The BBC micro:bit is currently only available for sale in the UK through Farnell element14, CPC and our approved re-sellers, but we've managed to secure ten devices to give away to members of our global community.

How to Enter

 

For your chance to get hold of one of these sought-after devices, simply read our 10 BBC micro:bit Projects in 10 Days series and 'like' your two favourite projects to earn the BBC micro:bit badge. Then, leave a comment under this blog telling us about a project you'd like to try out using the BBC micro:bit.

 

The ten participants who submit the best, most creative project ideas will each receive a BBC micro:bit and will be invited to write about their project here on element14.

 

Submissions are open until 23:59 (BST) on Sunday 31st July 2016. Full terms and conditions can be in the attached PDF.

 

To find out more about the BBC micro:bit initiative and the unique functionality of the device, visit the official BBC micro:bit website or read our exclusive interview with Premier Farnell's Strategic Alliance Director Richard Curtin.

Attachments:
image10 BBC microbit projects in 10 days Terms Conditions.pdf
  • Sign in to reply

Top Comments

  • jlucas
    jlucas over 10 years ago +7
    Thanks for all of your submissions guys, some really excellent project ideas here. I'm happy to announce that the following ten members have been selected to receive a BBC micro:bit device to undertake…
  • dougw
    dougw over 10 years ago +5
    I have been intrigued with the BBC micro:bit since it was announced last year. It represents a very ambitious and visionary initiative to boost interest in technology and computing. I suspect the dividends…
  • jlucas
    jlucas over 10 years ago +4
    Apologies for the delay guys. We had some shipping issues but these are now resolved and we'll be sending them out this week. Looking forward to seeing all of your projects.
  • beacon_dave
    beacon_dave over 10 years ago in reply to jc2048

    There may be scope for two science interfaces here. One bench-top design for classroom science lab type use that can be easily connected up to existing lab type equipment and then a low cost handheld 'multimeter/logger' type one for use by the pupils for measuring and logging data outside of the classroom in field/home environments.

     

    One aspect to consider perhaps is the final transfer of the logged data and how this is recorded longer term. I can still remember having to cutting up ticker tape and tape/glue it into my Physics workbook in order to keep a record of the experiment data for later revision purposes. With a data logger however, may need to consider some sort of till roll type printer attached to the science interface in order to quickly allow the pupils to get a hard copy that can be taped into their workbooks.

     

    Similar with a portable science interface. If we are going to encourage the class to start data logging in the field, then there will need to be some mechanism to off-load and archive that data somehow for later analysis and sharing or inclusion in a project report.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jc2048
    jc2048 over 10 years ago in reply to shabaz

    OK. When they become available to buy, I promise I'll get one and do a project with it. Not necessarily the whole of the science interface, though (to do that properly, as a complete, integrated package, would take much more skill and effort than I could throw at it).

     

    Nice name. You're much better tuned to a young audience than I am. micro:lab might work too. It carries some of the same ideas as 'professor' suggests.

     

    Perhaps the micro:professor could have an electron wizzing round her head. [I presume she has to wear a lab coat and glasses as per the regular stereotype.] I'm determined to get an electron in the branding somehow or other.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago

    The big idea I would like to introduce is Telemetry, the remote monitoring of environment and equipment that forms the basis of industrial and environmental control systems. I would do this by making use of the micro:bits internal temperature sensor and then the built in wireless messaging.

     

    So initially read the internal temperature as an expedient surrogate for an external sensor such as (DS18B20) which can be added later. The internal temperature actually gives a good approximation of the external air temperature for a pausing loop, on an exposed board. Display this across the scrolling 5x5 display and illustrate use through a glass window reading the display from inside. I can display in both Centigrade and Fahrenheit under programmable button control. Now what if we wanted to monitor it from our desk (in bluetooth radio range). We use a second micro:bit and the very cool radio messaging. A very simple yet functional demo.

     

    We can then use a twisted pair between two I/O pins on both micro:bits and illustrate how a longer line, possibly differentially driven, can be used to communicate. This could monitor near freezing temperatures in a garage, or the need to open venting windows of a greenhouse. The project can then be extended to add multiple sensor units, or control via a remote point, for example to operate an additional terrarium lamp when the temperature drops. The extension possibilities are endless. The concept is remote measurement.

     

    I have read the terms and conditions and am able to build the above, video, post etc.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 10 years ago in reply to jc2048

    I think you'll love it.

    I was also impressed that it is possible to go from opening the packaging and connecting it, to writing a short program or editing a hello world one, and downloading it, and running it, all in 60 seconds. (I'm not exaggerating : ) it was actually under 60 seconds.

     

    The science interface is a great idea.

    How about micro:professor? Since it helps kids to do experiments and makes them all micro-experts in scientific areas. (derived from the TI Little Professor that helped to teach a generation too : ).

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 10 years ago in reply to jc2048

    There was a Theremin project for the Arduino

    Open.Theremin.UNO - The real Theremin on Arduino

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>