Tech Connection
  • Learn
  • Learning Center
  • Tech Connection
  • More
  • Cancel
Tech Connection
Blog How do you Transfer Signal and Power Between Isolated Circuits?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Tech Connection to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Toptech-Voices
Engagement
  • Author Author: dychen
  • Date Created: 22 Feb 2024 5:16 PM Date Created
  • Views 19031 views
  • Likes 4 likes
  • Comments 1 comment
  • icoupler
  • adi
  • power supply
  • tech spotlight
  • isolation
  • analog devices
  • digital isolator
  • noise
  • isopower
  • microtransformer
  • safety
Related
Recommended

How do you Transfer Signal and Power Between Isolated Circuits?

dychen
dychen
22 Feb 2024

By Baoxing Chen

imageIn a circuit, different parts are typically isolated from one another to improve data integrity and safety. Unwanted signals can be generated by the circuit's power supply. Without isolation, these signals can leak into the rest of the circuit, causing noise and other anomalies. Additionally, isolation protects components and users from the potentially dangerous voltages in the power section.

Isolation is often achieved using optocouplers, however, even with modern technology, transmitting power from the non-isolated side to the isolated side remains a challenge. In this article, Analog Devices Fellow Baoxing Chen discusses how to use isoPowerTm and microtransformer technology to solve this problem.

Isolation between circuit components is typically required for safety and/or data integrity considerations. For example, isolation protects sensitive circuit components and human interface on the system side from dangerous voltage levels present on the field side, where more robust components such as sensors and actuators reside. Isolation can also eliminate common-mode noises or ground loops that affect data acquisition accuracy. While data transfer across an isolation barrier can be achieved through traditional optocouplers or Analog Devices iCoupler devices, the main challenge and common headache has been to find a way to transmit power from the nonisolated system side to the isolated field side. This paper discusses the technology behind a new approach that addresses this challenge by integrating power supply isolation with data signal isolation using Analog Devices’ latest iCoupler products.

Until recently, transferring power across an isolation barrier required either a separate dc-to-dc converter, which is relatively large, expensive, and has insufficient isolation, or a custom discrete approach, which is not only bulky but also difficult to design.

These approaches have been the only viable alternatives, even in applications such as data acquisition modules where only small levels of isolated power are needed.

Analog Devices has recently addressed this issue with the introduction of a complete and fully integrated isolation solution involving signal and power transfer across an isolation barrier using microtransformers. This extension to our iCoupler technology, termed isoPower, is a breakthrough alternative. Signal and power within a single component eliminates the need for a bulky, expensive, difficult to design isolated power supply and provides adequate isolation up to 5 kV. It can significantly reduce the total isolation system cost, the board space, and design time. A 2-channel iCoupler device with isoPower as shown in Figure 1 is almost 90% smaller and 70% less expensive.

image

Figure 1. Cost and size comparison between traditional approach and isoPower approach.

iCoupler Technology with isoPower

The integration of dc-to-dc converters involves the use of transformer switches, rectification diodes, and most importantly, a transformer. Reducing the size of the transformer to enable its integration in a complete isolation solution is made possible by using high switching frequencies, on the order of 300 MHz. This runs counter to the approach used in magnetic core transformers where the permeability of the magnetic core starts to degrade at high frequencies, leading to appreciable core loss that lowers efficiency. In addition, a magnetic core could also compromise the isolation rating of the transformers. Coreless iCoupler transformers, on the other hand, can be switched at higher frequencies and are much simpler to implement.

The microtransformers used in iCoupler devices are built on top of a CMOS substrate. Figure 2 shows a cross section of the isolated transformer structure, and Figure 3 is a die photo with both power and signal transformers. The transformer series resistance is minimized through the use of 6 μm thick plated Au for both the primary and the secondary spirals. The 20 μm thick polyimide in between the primary and the secondary provides HV isolation up to 5 kV. The additional 5 μm thick polyimide under the bottom spiral helps to reduce substrate capacitance and substrate loss. The substrate loss is further reduced through a carefully designed patterned ground shield using available underlying IC metal. The proximity effect and eddy current loss is less of a concern for the stacked transformers with large magnetic coupling coefficient. The design of the coils can be done through the optimization of coil parameters, such as the number of turns, trace width, and trace pitch. The quality factor (Q) at 300 MHz can be as high as 20 for the top coil and 15 for the bottom coil. The high Q for the microtransformer structure makes an efficient power transfer possible.

image

Figure 2. Cross section of iCoupler transformer coil.

image

Figure 3. Photograph of transformer die showing the power transformer coil and the two data transformer coils.

The transfer of the digital signal is realized through transmitting short pulses approximately 1 ns wide across the transformers with two consecutive short pulses to indicate a leading edge and a single short pulse as a falling edge. Figure 4 shows the signal transfer block diagram. A nonretriggerable monostable at the secondary generates detection pulses. If two pulses are detected, the output is set to high. On the other hand, if a single pulse is detected, the output is set to low. An input filter helps to increase noise immunity. The dc correctness is guaranteed by refresh signals sent into the transformers when no signal edges are detected for about 1 μs. If the input is high, two consecutive short pulses are generated as refresh pulses, and if the input is low, refresh of a single short pulse is generated. To complement the refresh circuit on the driver side, a watchdog is implemented in the receiver to make sure the output is at a fail-safe state when no refresh pulses are detected.

image

Figure 4. Digital signal transfer block diagram.

Similar microtransformers are used to transfer power. Because of their small L/R ratio, the transformers need to be switched at a high frequency to avoid current saturation and to achieve high efficiency. An example of four complementary CMOS switches implemented in a cross-coupled configuration together with the transformer forming sustaining oscillation is shown in Figure 5. The tank component sizes are optimized to maximize the energy transfer efficiency. The integrated Schottky diodes were used as rectification devices. These diodes turn on and recover fast enough for 300 MHz rectification. The diodes need to be sized such that they stay in Schottky region during rectification. A linear regulator on the secondary maintains the output voltage with output load or input supply variations. Efficiency is less of a concern for many low power applications. To improve efficiency and maintain energy regulation, an optional feedback signal transformer can be added. The feedback signal would turn on/off the LC tank instead of controlling the transformer switches directly. This approach separates the energy regulation from energy conversion, allowing optimized power transfer and maintaining regulation.

image

Figure 5. Power transfer block diagram.

One common concern about switching transformers is their electromagnetic interference, particularly for a transformer switching at 300 MHz. Using the far-field approximation,

image

 The wavelength, λ, at 300 MHz is about 1 meter, the transformer with a radius in the range of 0.5 mm is still a very poor antenna with a small r/λ. It is estimated that the total radiated power is still less than 500 pW even if the part is operating at 300 MHz with a loop current of 350 mA. The near-field radiation drops rapidly with the distance from the transformer. The on-chip transformers are only closely coupled with a small separation, 20 μm in this case.

Example Application: The ADuM5242 in a Secondary Control Power Supply

Digital Isolators

Shop our wide variety of Digital Isolators from Analog Devices.

Shop Now


Don't forget to join our discussion.

Secondary control architectures have gained traction as new power supplies trend toward lower supply voltage, faster dynamic response, and more system interaction between the supply and the load. There are two main difficulties in adopting secondary control vs. primary control. The first is the need for high performance digital isolation vs. analog isolation. An inexpensive analog optocoupler is typically used to send analog feedback error signal from the secondary to the primary in a system with primary control, while an expensive or bulky digital coupler would be needed to send PWM signals across the isolation barrier for a system with secondary control.

The second difficulty is the need for power at the secondary controller before the system has started up. The primary controller has no such issue, as power is always available at the primary side. There are two ways to solve this secondary control start-up issue. One method is to add an auxiliary power supply exclusively for the secondary controller startup. A second method is to have a dedicated start-up component on the primary side to build initial bias at the secondary for the start up of secondary controller.

Analog Devices’ ADuM5242, a dual-channel digital isolator with a 50 mW isolated output, is an ideal solution to the start-up problem. This 8-lead SOIC component provides two isolation channels that support PWM signals up to 10 Mbps and 10 mA of 5 V isolated power for the start up of the secondary controller. The user has the further option of disabling the power once the system is started up. The disable is achieved through monitoring the input supply voltage. When the input supply drops below 4 V, the feedback control switch shown in Figure 5 is turned off. Figure 6 is an example application block diagram showing the ADuM5242 in a secondary control system. The two digital signal channels provide the feedback signals from the secondary controller with synchronous rectification to drive the half-bridge drivers at the primary.

image

Figure 6. Example of secondary control system employing ADuM5242 with isoPower.

Together with ADuM5242, two other data channel configurations have also been introduced. The ADuM5240 has two isolated output channels, while the ADuM5241 has one isolated output and one isolated input. This provides the flexibility to support a wide variety of applications. The ADuM524x products can also be used in combination with other multichannel iCoupler devices to configure higher quantities of isolated signal channels.

image
ADuM5242 Digital Isolator
Buy Now
image
ADuM5241 Digital Isolator
Buy Now
image
ADuM5240 Digital Isolator
Buy Now

Summary

In partnership with

logo

iCoupler technology with isoPower provides a complete isolation solution within a single package. Not only does it offer state-of-the-art digital signal isolation having substantial advantages over optocouplers in terms of power, size, and performance, but it also eliminates the need for a separate, isolated power supply. The iCoupler technology provides unprecedented possibilities for functional integration that can dramatically reduce the complexity, size, and total cost of the isolated systems.

Join our Discussion!

What types of problems have you encountered in the past due to a lack of isolation?

Please tell us in the Comments section below.

  • Sign in to reply
Parents
  • SigmaPrimus
    SigmaPrimus over 2 years ago

    Will we be seeing Buck/Boost converters using this technology soon?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • SigmaPrimus
    SigmaPrimus over 2 years ago

    Will we be seeing Buck/Boost converters using this technology soon?