Tech Connection
  • Learn
  • Learning Center
  • Tech Connection
  • More
  • Cancel
Tech Connection
Blog How Does a Silicon Photomultiplier Work?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Tech Connection to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
EMI-Reduction-Techniques
Engagement
  • Author Author: dychen
  • Date Created: 19 Dec 2023 3:37 PM Date Created
  • Views 22550 views
  • Likes 4 likes
  • Comments 2 comments
  • Single Photon Avalanche Diode
  • light detector
  • photodiode
  • sensitivity
  • lidar
  • tech spotlight
  • pmt
  • dark noise
  • silicon photomultiplier
  • SiPM
  • photomultiplier
  • photodetector
  • microcell
  • spad
  • broadcom
Related
Recommended

How Does a Silicon Photomultiplier Work?

dychen
dychen
19 Dec 2023

imageA silicon photomultiplier, or SiPM, is a solid-state photodetector that is used to detect and quantify light signals. They are particularly sensitive to low levels of light and are used in applications where precise and sensitive light detection is required. An SiPM is based on the principle of avalanche photodiodes, consisting of an array of small, interconnected silicon photodiodes (also known as pixels or microcells) that are operated in reverse bias. Each individual pixel can detect a single photon and when a photon is absorbed by a pixel, it triggers an avalanche-like multiplication of charge carriers, which results in a measurable electrical signal. The output of the SiPM signal is an electrical current proportional to the number of photons hitting the sensor. The result is a high-gain signal (>1 x 106) with fast reaction and recovery times.

SiPMs are used in a variety of applications due to their exceptional sensitivity and versatility. They are commonly used in industries utilizing light detection and ranging (LiDAR) or radiation detection. SiPMs are also have applications in X-ray and gamma-ray detection, nuclear medicine, positron emission tomography (PET), safety, security, and Cherenkov detection applications.

Advantage of Silicon Photomultipliers

SiPMs have distinct advantages over traditional light detectors:

  • SiPMs are highly sensitive and can detect individual photons, even in low-light conditions.
  • The fast response time of SiPMs has made them invaluable for applications with an emphasis on precision timing.
  • The compact size of SiPMs makes them ideal for space-constrained or portable applications.
  • SiPMs are not influenced by magnetic fields, making them crucial for applications like magnetic resonance imaging (MRI).
  • SiPMs have a wide spectral range, from ultraviolet to near-infrared.
  • SiPMs can operate at low voltages, making them extremely energy efficient.

How do SiPMs Compare to Conventional Light Detectors (Photodiodes)? 

SiPMs and conventional photodiodes are both photodetectors, but they differ in several key aspects. Photodiodes produce one electron and one hole for each incident photon, yielding a signal that can be overshadowed by intrinsic noise. Photodiodes have low gain, lack carrier multiplication, and provide limited signal amplification. When operating below the breakdown voltage, they exhibit a low excess noise factor. Their output signal is linearly proportional to the number of incident photons within a large intensity-range.

In contrast, when a photon strikes an SiPM, it can trigger an avalanche of carriers, allowing a single photo-generated carrier to generate a significant number of internal carriers, resulting in substantial signal amplification. Due to statistical carrier multiplication, SiPMs can amplify signals significantly, although this may introduce higher noise levels. If SiPMs operate beyond their breakdown voltage, they exhibit a self-sustaining avalanche effect, but a quenching resistor can reset the device within tens of nanoseconds after an avalanche event. An SiPM operates above its breakdown voltage, the voltage at which the electric field across the detector becomes strong enough to cause a sustained discharge or avalanche of charge carriers. This operational mode is referred to as Geiger mode. As a result, an SiPM produces a consistent output signal regardless of the photon count, making them ideal for photon-counting applications. They can also be arrayed to enhance performance, making them a preferred choice for sensitive and reliable photon detection in various applications.

What is the Difference Between an SiPM and a PMT?

Photomultiplier tubes (PMTs) are encased in fragile and bulky housing, with other limitations, including vulnerability to ambient light, sensitivity to magnetic fields, and the requirement for high voltage. These limit their adaptability in various applications. SiPMs present a more modern and versatile solution. They are resistant to ambient light and interference, housed in compact and robust enclosures suitable for handheld devices, and are unaffected by magnetic fields. They operate at a lower bias voltage and consume less power, in addition to offering higher light sensitivity and excellent timing performance. Furthermore, SiPMs support the construction of high granularity arrays, making them the preferred choice in applications that demand fast timing, high sensitivity, robustness, and compactness. A more detailed comparison of the two is shown in Table 1.

Characteristic

Silicon Photomultiplier (SiPM)

Photomultiplier Tube (PMT)

Sensitivity

Single photon

Single photon

Gain

To

To

Large area

Yes, scalable

Yes

Operation voltage

30V to 50V

800V to 2000V

High-density arrays

Yes

No

High granularity/ resolution

Yes

No

Dark noise

Fair

Low

Response time

Very Fast

Fast

Uniformity

Excellent

Good

Photon-counting resolution

Excellent

Good

Temperature sensitivity

Medium

Low

Immunity to ambient light

Yes

No

Immunity to a magnetic field

Yes

No

Compactness and lightweight

Yes

No

Table 1: PMT and SiPM Comparison

How does a Silicon Photomultiplier work?

Photomultipliers

Shop our wide variety of Silicon Photomultipliers (SiPM) from Broadcom.

Shop Now


Don't forget to join our discussion.

SiPMs comprise arrays of avalanche photodiodes, often referred to as Single-Photon Avalanche Diodes (SPADs). They are designed to detect very low levels of light, down to a single photon. Depending on the light source and application, several hundred to thousands of SPADs can be connected parallel to form a SiPM array. Each SPAD in a SiPM includes an integrated series resistor that quenches the avalanche and resets the diode for the next incoming photon.

SPADs always produce the same output signal in Geiger-mode operation, regardless of the number of photons that initiate the avalanche. SPADs are binary – either ON or OFF. Multiple SPADs are often arranged in an array and connected in parallel (as shown in Figure 1), creating an SiPM array or silicon photomultiplier (SiPM) that can overcome this restriction and provide a more versatile output response to the number of detected photons.

SPAD SiPM

Figure 1: Schematic of a SPAD Arrangement and SiPM Signal Formation (Source: Broadcom)

What is the Basic Electrical Model of an SiPM?

Figure 2 depicts the basic electrical model of an SiPM electrical model. The key parameters of the model are Cd: capacitance of the single SPAD, Rq: quenching resistor, Cq: the parasitic capacitance of the quenching resistor, and Cg: the parasitic capacitance of the grid.

SiPM Model

Figure 2: The Basic Model of an SiPM (Source: F. Corsi et al., Nuclear Instruments and Methods in Physics Research, 2007.)

What is Dark Noise (or Dark Rate) in an SiPM?

Dark noise, also known as dark count or dark rate, in a Silicon Photomultiplier (SiPM) refers to the unwanted or spurious electrical pulses generated by the SiPM in the absence of incident light. It represents the intrinsic noise level of the SiPM when no photons are striking the device. Dark noise makes it difficult to detect photons, especially in low light levels. It is primarily caused by thermal generation of carriers in the avalanche region  can also be caused by defects or traps in the silicon material, which can capture and release charge carriers.

How to Select SiPMs for Specific Applications

Figure 3 depicts a decision tree used to determine the suitability of an SiPM for a specific application. This decision is based on several factors, including the wavelength of light to be detected, the type of light source (pulsed/continuous), the light intensity, and the frequency of light pulses. Depending on these factors and the specific application, the readout solution can be either a photon/pulse counting, a charge integration, or a combination of both.

SiPM Application Decision Tree

Figure 3: SiPM Application Decision Tree

SiPMs are well-suited for photodetection tasks, provided the application meets the requirements. These requirements may include geometrical considerations (photosensitive area, device volume), resistance to ambient light, the number of detection channels, granularity (number of channels per unit area), susceptibility to magnetic fields, or mechanical ruggedness.

Silicon Photomultipliers from Broadcom

Broadcom offers a diverse range of SiPMs tailored to various applications, including the new NIR30, designed for LiDAR applications and offer best-in-industry sensitivity at 905nm and 940nm.

image
Silicon Photomultiplier, 3.72mm x 3.72mm, 30µm/15060 Microcells, 420nm
Buy Now
image
Silicon Photomultiplier Array, 4x1, 3.72mm × 3.62mm, 40µm/8334 Microcells, 420nm
Buy Now
image
Silicon Photomultiplier Array, 2x1, 13.54mm x 6.54mm, 40µm/22428 Microcells, 420nm
Buy Now
image
Silicon Photomultiplier, 3.72mm × 3.62mm, 40µm/8334 Microcells, 420nm
Buy Now
image
Silicon Photomultiplier, 6mm x 6mm, 40µm/22428 Microcells, 420nm
Buy Now

Summing up: Detecting Light with Silicon Photomultipliers

In partnership with

logo

Silicon photomultipliers have revolutionized light detection across various industries. Their high sensitivity, fast response times, and immunity to magnetic fields make them ubiquitous in applications ranging from clinical imaging to high-electricity physics. SiPMs are expected to continue playing a significant role in future innovations involving the detection of light at radiation. Broadcom offers a comprehensive range of reliable SiPMs that are tailored for a variety of application.

Join our Discussion!

What new devices and applications do you think will be invented as photodetectors become smaller, more sensitive, and more accurate?

Please tell us in the Comments section below.

  • Sign in to reply
Parents
  • DAB
    DAB over 2 years ago

    Very interesting post.

    Your description of operation matches my theory on the photo-electric effect being based upon photon flow between atoms.

    Do you have any development boards that I could use with mircrocontrollers?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 2 years ago

    Very interesting post.

    Your description of operation matches my theory on the photo-electric effect being based upon photon flow between atoms.

    Do you have any development boards that I could use with mircrocontrollers?