Tech Connection
  • Learn
  • Learning Center
  • Tech Connection
  • More
  • Cancel
Tech Connection
Forum LED 4-Pin help needed
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Tech Connection to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 26 replies
  • Answers 15 answers
  • Subscribers 217 subscribers
  • Views 11232 views
  • Users 0 members are here
Related

LED 4-Pin help needed

hafcanadian
hafcanadian over 5 years ago

I could use some help choosing replacement 4-pin RGB lamps for my In Motion outdoor Xmas sets.  I have 20 twelve-lamp “C9” sets on the house, end to end, each with a control module.  They manage to stay in synch, so the modules must be absolutely identical electronically.  Color combinations and solids rotate in sequence and can be steady or flash, etc.  The colors include white, purple, orange, etc., not just RGB, so the controllers apparently mix RGB with varying current I assume.

 

When new I had sets that acted up, with sections of 3 or 4 lights staying solid white, or occasionally groups of lamps entirely out.  The mfr. ultimately sent me more than 20 new sets, so usually now I just replace an entire faulty string with one of those, and later try to fix the original.  But that’s a nightmare, and I now have 7 or 8 sets from years past clogging my workbench.  Sometimes just juggling lamp positions works, but usually it’s a bugger ferreting out what’s wrong.  It’s easy to suspect the controllers, but sometimes just replacing just the right lamp with a spare does the trick.  But because there are 4 wires instead of just 2, I have a devil of a time finding the faulty lamp;  my yellow LED Xmas gun isn’t useful on controlled 4 pin lamp sets.

 

Since there only 2 spare lamps in holders with each set (and some sets had no spares), I’d like to get spare 4-pin bulbs.  If I just replace lamps one at a time until a set works, since they fail in straight groups of 3, that may be easiest.   The pins are too long and often need trimming a bit to fit the holder or they jam going into the sockets.  Problem is I’m not sure which lamp to order.  Maybe you can assist.  The tag on each cord says to replace with 3v fuses, and 4v. 0.25 w lamps.  That’s it.  In searching online I see options on Amazon (Chanzon), but they are clear lenses and mine are diffused.  The ones at Amazon say 3v.  More concerning is they come either common anode or common cathode, and I don’t know how to tell which that mine are.  They are domed 5mm.  I looked at Mouser.com but was still left with uncertainty.

 

Can you advise?  I’d sure like to clear these 7 or 8 sets off my garage workbench, and for once have room for other projects as they come up!

Thanks,

Joel

Clackamas, Oregon

  • Sign in to reply
  • Cancel

Top Replies

  • fmilburn
    fmilburn over 5 years ago +4 suggested
    Hi Joel, it is difficult to answer your question with the information provided. By the way, you need only post it once. Posting a photo of the lamps could be helpful. I Suggest starting with some simple…
  • ralphjy
    ralphjy over 5 years ago in reply to hafcanadian +4 suggested
    I think that this tutorial should help you. It explains the pinout and different methods of controlling the colors. https://www.circuitbread.com/tutorials/how-rgb-leds-work-and-how-to-control-color Ra…
  • fmilburn
    fmilburn over 5 years ago in reply to hafcanadian +4 suggested
    The video that Ralph linked appears to go into more depth and will provide useful information. The language on the tag is confusing. The LEDs don't really work at 4V or for that matter 3V. Depending on…
Parents
  • fmilburn
    0 fmilburn over 5 years ago

    I am going to speculate a bit here.

     

    The LEDs have the following characteristics:

    • They don't behave like a traditional "dumb" RGB LED
    • They have the same length leads as an APA-106 and the same flat edge on the side
    • From my testing the GND pin and VDD seem to be the same as an APA-106
    • Adafruit sell something similar that is said to work with their NeoPixel library
    • The Adafruit NeoPixel library for the WS2812 doesn't quite work with these LEDs

     

    I remember reading about a change to the WS2812 and found this May 2017 post which references WorldSemi:  Heads up – WS2812B NeoPixels are about to change! – Particle Blog.  In the 2017 article they state that:

     

    According to WorldSemi, the new WS2812B NeoPixels have a longer required reset interval, up to 280us from 50us.

    They go on to say that their product would not light the WS2812Bs as a result.  What may be happening is that Joel's LEDs use the old reset interval of 50 us and the NeoPixel library uses the newer interval.  When I hold my finger just so (it doesn't always work) I may be changing the capacitance or something that changes the reset duration and allows it to turn on but they still don't function properly.  I have the Arduino in a loop sending a new signal each pass and it turns off when I pull my finger away.

     

    Some years ago I wrote a driver for the WS2812 and a MSP430 microcontroller.  I suppose I could dig out that code and modify it as necessary to change the reset period and test a lamp or we could use a logic analyzer or oscilloscope to determine what the reset period coming out of the TY-16F is and whether it matches the APA-106 protocol.  But I am not sure how much good that would do if the older lamps are obsolete and can't be found.

     

    Assuming these are old APA-106 with a shorter reset duration I am running out of ideas other than ordering some new APA-106 and seeing if they work with the controller.  Small quantities are available on Tindie and probably elsewhere.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • fmilburn
    0 fmilburn over 5 years ago

    I am going to speculate a bit here.

     

    The LEDs have the following characteristics:

    • They don't behave like a traditional "dumb" RGB LED
    • They have the same length leads as an APA-106 and the same flat edge on the side
    • From my testing the GND pin and VDD seem to be the same as an APA-106
    • Adafruit sell something similar that is said to work with their NeoPixel library
    • The Adafruit NeoPixel library for the WS2812 doesn't quite work with these LEDs

     

    I remember reading about a change to the WS2812 and found this May 2017 post which references WorldSemi:  Heads up – WS2812B NeoPixels are about to change! – Particle Blog.  In the 2017 article they state that:

     

    According to WorldSemi, the new WS2812B NeoPixels have a longer required reset interval, up to 280us from 50us.

    They go on to say that their product would not light the WS2812Bs as a result.  What may be happening is that Joel's LEDs use the old reset interval of 50 us and the NeoPixel library uses the newer interval.  When I hold my finger just so (it doesn't always work) I may be changing the capacitance or something that changes the reset duration and allows it to turn on but they still don't function properly.  I have the Arduino in a loop sending a new signal each pass and it turns off when I pull my finger away.

     

    Some years ago I wrote a driver for the WS2812 and a MSP430 microcontroller.  I suppose I could dig out that code and modify it as necessary to change the reset period and test a lamp or we could use a logic analyzer or oscilloscope to determine what the reset period coming out of the TY-16F is and whether it matches the APA-106 protocol.  But I am not sure how much good that would do if the older lamps are obsolete and can't be found.

     

    Assuming these are old APA-106 with a shorter reset duration I am running out of ideas other than ordering some new APA-106 and seeing if they work with the controller.  Small quantities are available on Tindie and probably elsewhere.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer