Tech Connection
  • Learn
  • Learning Center
  • Tech Connection
  • More
  • Cancel
Tech Connection
Forum LED 4-Pin help needed
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Tech Connection to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 26 replies
  • Answers 15 answers
  • Subscribers 217 subscribers
  • Views 11225 views
  • Users 0 members are here
Related

LED 4-Pin help needed

hafcanadian
hafcanadian over 5 years ago

I could use some help choosing replacement 4-pin RGB lamps for my In Motion outdoor Xmas sets.  I have 20 twelve-lamp “C9” sets on the house, end to end, each with a control module.  They manage to stay in synch, so the modules must be absolutely identical electronically.  Color combinations and solids rotate in sequence and can be steady or flash, etc.  The colors include white, purple, orange, etc., not just RGB, so the controllers apparently mix RGB with varying current I assume.

 

When new I had sets that acted up, with sections of 3 or 4 lights staying solid white, or occasionally groups of lamps entirely out.  The mfr. ultimately sent me more than 20 new sets, so usually now I just replace an entire faulty string with one of those, and later try to fix the original.  But that’s a nightmare, and I now have 7 or 8 sets from years past clogging my workbench.  Sometimes just juggling lamp positions works, but usually it’s a bugger ferreting out what’s wrong.  It’s easy to suspect the controllers, but sometimes just replacing just the right lamp with a spare does the trick.  But because there are 4 wires instead of just 2, I have a devil of a time finding the faulty lamp;  my yellow LED Xmas gun isn’t useful on controlled 4 pin lamp sets.

 

Since there only 2 spare lamps in holders with each set (and some sets had no spares), I’d like to get spare 4-pin bulbs.  If I just replace lamps one at a time until a set works, since they fail in straight groups of 3, that may be easiest.   The pins are too long and often need trimming a bit to fit the holder or they jam going into the sockets.  Problem is I’m not sure which lamp to order.  Maybe you can assist.  The tag on each cord says to replace with 3v fuses, and 4v. 0.25 w lamps.  That’s it.  In searching online I see options on Amazon (Chanzon), but they are clear lenses and mine are diffused.  The ones at Amazon say 3v.  More concerning is they come either common anode or common cathode, and I don’t know how to tell which that mine are.  They are domed 5mm.  I looked at Mouser.com but was still left with uncertainty.

 

Can you advise?  I’d sure like to clear these 7 or 8 sets off my garage workbench, and for once have room for other projects as they come up!

Thanks,

Joel

Clackamas, Oregon

  • Sign in to reply
  • Cancel

Top Replies

  • fmilburn
    fmilburn over 5 years ago +4 suggested
    Hi Joel, it is difficult to answer your question with the information provided. By the way, you need only post it once. Posting a photo of the lamps could be helpful. I Suggest starting with some simple…
  • ralphjy
    ralphjy over 5 years ago in reply to hafcanadian +4 suggested
    I think that this tutorial should help you. It explains the pinout and different methods of controlling the colors. https://www.circuitbread.com/tutorials/how-rgb-leds-work-and-how-to-control-color Ra…
  • fmilburn
    fmilburn over 5 years ago in reply to hafcanadian +4 suggested
    The video that Ralph linked appears to go into more depth and will provide useful information. The language on the tag is confusing. The LEDs don't really work at 4V or for that matter 3V. Depending on…
Parents
  • fmilburn
    0 fmilburn over 5 years ago

    jw0752

    dougw

    ralphjy

     

    I am hoping you might be able to help with this...  I had Joel send me two of his RGB LEDs described above and I attached them to my bench power supply assuming the long lead was cathode.  I set the maximum current to 3 mA and then increased the voltage to the red lead.  On the first LED I got a dim red response at about 2.4V and then the LED went out.  The green and blue did not light at all but I could get current across them.

     

    Thinking it was a bad LED I hooked up the second one.  This time I got a brighter response and took a photograph.  See the image below...

    image

    The LED on the right is the one from Joel.  The one on the left is a fresh one that was in my box of LEDs.  You can see my LED is much brighter than the one from Joel at the same current and it turns on at a lower Vf.  I couldn't get the green or blue on the second LED from Joel to turn on (mine worked as expected).  Then I tried the red on Joel's again and now it won't light.  I guess I fried it at 3 mA.

     

    So I don't have an idea of what is happening.  It appears the long lead is cathode and red is in the same location as my LED.  Joel sent me LEDs that were working in his string but they appeared to burn out at only 3 mA in my test.  Any ideas?  I was thinking I might send him some of mine that he could try in his string.

     

    Thanks for any help image

    Frank

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • fmilburn
    0 fmilburn over 5 years ago in reply to fmilburn

    Here is what I know now....

     

    I hooked up an Arduino Uno using 5V as power and the Adafruit Neopixel library.  I tested it on a known good WS2812 to make sure it worked.  The APA-106 is supposed to use the same protocol as the WS2812.  Then I hooked up one of Joel's LEDs using the pinout of the APA-106.  It wasn't lit so I jiggled it around with my finger and lo and behold it lit extremely brightly.  When I pulled my finger away it turned off.  So I put my finger back on and held it a second or two but it started smoking.  Obviously there was no current limiting / PWM.  One down, one more to go :-).  I stuck the other one in and it didn't light.  So I jiggled it with my finger and it lit.  I immediately pulled my finger away and it turned off.  Put it back on and it lit, immediately pulled away. I entertained myself that way a couple more times and stopped while it was still working.  Next time I will put a resistor in series.

     

    image

     

    I could have it wrong but I have double checked the wiring and believe it to be correct for an APA-106.  I am going to put it aside for the evening and think about it some more.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • hafcanadian
    0 hafcanadian over 5 years ago in reply to fmilburn

    Sounds like you fellows are zeroing in on the right lamp.  The parameters I read for the APA-106 was darned close to what the light set’s instruction sheet calls for as replacements.  0.24 watt, 4 volts.  The APA-106 specs I saw are 0.24 w, 4.5-6 v.  Don’t know how critical that 4 volts specification is.

     

    I sure appreciate your effort and capabilities.  So the dark shadow inside the diffused “lens” is a tiny built-in controller c.b.?  I didn’t know there was such an animal.  The TY-16F must have the resistor? 

     

    I believe I’d earlier mentioned that I’d thought the mfr. had trimmed the pins to fit their holder, so when bent over their tips didn’t overlap the holder and jamb when inserted in the socket.  But I note the lamps have 2 long and 2 short pins, unlike regular ones.  The pins in mine probably weren’t trimmed after all.

     

    Joel

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • fmilburn
    0 fmilburn over 5 years ago in reply to hafcanadian

    Assuming the lamps are APA-106, then the TY-16F is a controller that sends signals to the individual lamps.  It would not have a resistor because the microcontroller in the individual lamps will use pulse width modulation (PWM) to turn the lamps on and off quickly so that the averaged current appears to dim the LEDs to our eyes (we don't see the flicker) and also keeps them from burning out.  It is useful to know that the LEDs in your possession have two long and two short pins like the APA-106.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • fmilburn
    0 fmilburn over 5 years ago in reply to hafcanadian

    Assuming the lamps are APA-106, then the TY-16F is a controller that sends signals to the individual lamps.  It would not have a resistor because the microcontroller in the individual lamps will use pulse width modulation (PWM) to turn the lamps on and off quickly so that the averaged current appears to dim the LEDs to our eyes (we don't see the flicker) and also keeps them from burning out.  It is useful to know that the LEDs in your possession have two long and two short pins like the APA-106.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer