Tech Connection
  • Learn
  • Learning Center
  • Tech Connection
  • More
  • Cancel
Tech Connection
Forum What Key Lessons Should We Be Learning about Renewable Energy?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Tech Connection to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 213 subscribers
  • Views 2337 views
  • Users 0 members are here
  • What Key Lessons Should We Learning about Renewable Energy?
Related

What Key Lessons Should We Be Learning about Renewable Energy?

rscasny
rscasny over 4 years ago

We just published a new spotlight article called How Do You Make The Most of Renewable energy?

The article covers a variety of things about it, as well as some key points about power switching. 

Do you have any lessons you have learned as you try to apply renewable energy in your home and business life?

  • Sign in to reply
  • Cancel

Top Replies

  • ralphjy
    ralphjy over 4 years ago +3
    The increased push toward electric vehicles and increasing stress on the power grid due to a variety of issues have made me want to add battery storage to my solar installation. The recent passage of the…
  • kmikemoo
    kmikemoo over 4 years ago in reply to ralphjy +3
    ralphjy I know that you will, but please do your research before you purchase a battery storage solution. I have two different sets here at work and they are vastly different although there is only a slight…
  • dougw
    dougw over 4 years ago +2
    Changing attitudes are half the battle. My better half no longer feels that solar panels are unacceptably ugly.
Parents
  • ralphjy
    ralphjy over 4 years ago

    The increased push toward electric vehicles and increasing stress on the power grid due to a variety of issues have made me want to add battery storage to my solar installation.  The recent passage of the “Inflation Reduction Act” in the US makes battery storage installations eligible for the 30% Federal Tax Credit.  I see batteries in the near future Relaxed.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • kmikemoo
    kmikemoo over 4 years ago in reply to ralphjy

    ralphjy  I know that you will, but please do your research before you purchase a battery storage solution.  I have two different sets here at work and they are vastly different although there is only a slight difference in price.

    One system really only charges from the grid while it's marketing material alludes to it charging from solar.  Sure your solar can be tied to the grid at the same time you are charging the batteries, but with no grid, your solar cannot charge your batteries.  When running from batteries, it must be the only source of power.  If you have to use a transfer switch... that is not the system I would recommend for you.

    The other system can use the batteries to mimic the grid and allow AC coupled solar to still function.  It can also call for generator - although it uses the generator in lieu of utility and solar.  Generators can't handle reverse power.

    All the battery storage systems I've researched require a sub-panel.  One thing I do not like about these systems is that they are not fail-safe.  When your inverter shuts down, you are isolated from ALL sources.  Darkness prevails.  Just some lessons from a guy that had to run back to work in the middle of the night a few times because the BMS shut the system down and it powered the furnace.  When it's single digit temperatures outside, it doesn't really matter if it's C or F.  You need heat.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • kmikemoo
    kmikemoo over 4 years ago in reply to ralphjy

    ralphjy  I know that you will, but please do your research before you purchase a battery storage solution.  I have two different sets here at work and they are vastly different although there is only a slight difference in price.

    One system really only charges from the grid while it's marketing material alludes to it charging from solar.  Sure your solar can be tied to the grid at the same time you are charging the batteries, but with no grid, your solar cannot charge your batteries.  When running from batteries, it must be the only source of power.  If you have to use a transfer switch... that is not the system I would recommend for you.

    The other system can use the batteries to mimic the grid and allow AC coupled solar to still function.  It can also call for generator - although it uses the generator in lieu of utility and solar.  Generators can't handle reverse power.

    All the battery storage systems I've researched require a sub-panel.  One thing I do not like about these systems is that they are not fail-safe.  When your inverter shuts down, you are isolated from ALL sources.  Darkness prevails.  Just some lessons from a guy that had to run back to work in the middle of the night a few times because the BMS shut the system down and it powered the furnace.  When it's single digit temperatures outside, it doesn't really matter if it's C or F.  You need heat.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Children
  • ralphjy
    ralphjy over 4 years ago in reply to kmikemoo

    Hi Mike,  I'll definitely do some research before choosing a battery solution.  I'll need to check with my local utility to see what they allow for grid reconnection after power loss.  I have a "Secure Power Supply" feature on my inverter to allow it to run when the grid is down, but I need to shut the inverter down before I reconnect after grid power is restored.  I know someone with a Tesla Powerwall (and a Tesla to go with it Smile), so I'll check with him to see how that setup works.

    The NEC will update next year, so I'll need to see if there will be new requirements.  The Rapid Shutdown Switch was a new requirement for 2017 and I had to order one at the last minute after all the other system components had delivered.

    I've thought about adding generator capability to power the house, but in that case I would probably just switch it in manually and not require it to charge the battery.  Probably the setup you described...

    Ralph