Publications
  • Learn
  • More
Publications
Blog A solution to EU Energy and Economic Crisis: Hybrid Power Plants
  • Blog
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Publications to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Eavesdropper
  • Date Created: 16 Dec 2011 8:22 PM Date Created
  • Views 661 views
  • Likes 1 like
  • Comments 2 comments
  • energy_savings
  • alternative_energy
  • hydrogen
  • industry
  • power_plant
  • prototyping
  • eavesdropper
  • hybrid
  • power
  • innovation
Related
Recommended

A solution to EU Energy and Economic Crisis: Hybrid Power Plants

Eavesdropper
Eavesdropper
16 Dec 2011
image
The energy cycle (via Vattenfall)
 
In a time when the European Union is in financial turmoil, German, French and Swedish companies are showing that there is the undeniable potential of renewable energies. Creating a small “ecosystem” of energies, each supporting or complementing the other is a clear example of what scientists and engineers are capable of when given the right resources and are not doubted by investors or restricted by money.
 
While there are many ways of generating renewably energy, engineers have had trouble finding ways to store excess energy. This has always been a drawback to obvious renewable-energy  solutions like wind energy. However, a new innovative power plant in Germany has found a solution.
 
Many European companies, including Vattenfall, Siemens, Enertrag along with research institutions and environmental organizations are behind a project that has been operating since October in Prenzlau Germany, 75 miles north of Berlin. Their project is in the form of a Hybrid power plant that solves the storage problem by converting electrical energy generated by with wind turbine, into hydrogen. 
 
A hybrid power plant is the first of its kind in Europe, consisting of three wind turbines, a biogas unit, an electrolysis unit and two combined power plants that make use of waste heat. 
 
The turbines are capable of delivering 2 MW of electricity. This electricity is then converted into storable hydrogen by the electrolysis, a process that been theorized to be 80%-94% efficient.  The hydrogen can be distributed via pipeline and used like natural gas for heat; it can fuel hydrogen vehicles, and it can also co-fire the power plant along with the biogas to produce more electricity exactly when it is needed.
 
Vattenfall Innovation head Oliver Weinmann stated their mission best, "There is currently no system designed to compensate for the differences between supply and demand within the sector of renewable energy... But this project allows us to find a balance in the system and it’s also good business.”
 
Eavesdropper
  • Sign in to reply
Parents
  • DAB
    DAB over 14 years ago

    They clearly understand to true issues in zero sum energy use.

    Until you do it and demonstrate to everyone that it can be done, the nay sayers will always say it can't be done.

    Once you demonstrate that the technology is cost effective, then they will say in might be done.

    After others begin to implement the technology on a broad scale, they will finally say it should be done.

     

    People are funny that way.  image

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Catwell
    Catwell over 14 years ago in reply to DAB

    So ture.

     

    Germany is running the show over there lately. If Germany -tells- others to build hybrid plants, those countries will reply "how many?"

     

    The benefits are multi-fold. Brute force creating of energy is becoming an old world idea. Efficient usage of every last Joule is becoming the status quo.

     

    Thankfully.

     

    Cabe

    http://twitter.com/Cabe_e14
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Catwell
    Catwell over 14 years ago in reply to DAB

    So ture.

     

    Germany is running the show over there lately. If Germany -tells- others to build hybrid plants, those countries will reply "how many?"

     

    The benefits are multi-fold. Brute force creating of energy is becoming an old world idea. Efficient usage of every last Joule is becoming the status quo.

     

    Thankfully.

     

    Cabe

    http://twitter.com/Cabe_e14