Publications
  • Learn
  • More
Publications
Blog Air Force creates solid-state quantum interferometer glass, quantum computing in mind
  • Blog
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Publications to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 20 Dec 2011 8:45 PM Date Created
  • Views 708 views
  • Likes 1 like
  • Comments 3 comments
  • quantum
  • cornell
  • quantum_computing
  • photonics
  • on_campus
  • interferometer
  • embedded
  • cabeatwell
  • prototyping
  • photon
  • university
  • innovation
Related
Recommended

Air Force creates solid-state quantum interferometer glass, quantum computing in mind

Catwell
Catwell
20 Dec 2011
imageimage
Depictions of the glass and how they can be stacked (via Cornell University white paper)
 
 
Interferometry is a technique where electromagnetic waves are superimposed to extract data from the wave itself. Using an interferometer is a device that does the job, refracting and reflecting photons, for example, to analyze the wave. The issue is that these apparatuses are delicate to say the least. Constant recalibration is needed. Interferometers are often used as a way to carry out quantum processing, where the output of one is the input of another.
 
Jonathan MacDonald and his team from the Air Force Research Laboratory in Rome New York, working alone with Cornell University, have developed a way to make interferometers more solid-state. Optigrate, common Holograms, interferometers are embedded in glass creating a high resistance to environmental changes. Which eliminates the need for calibration. MacDonald stated that this tech could perform quantum teleportation and CNOT logic.
 
Unfortunately, the quantum glass is not reprogrammable. Each pane would be crafted to perform a single operation. If nothing else, the tech will speed up experimentation in quantum research.
Read more in the "Quantum Computing in a Piece of Glass" white paper.
 
I think the Air Force should look at the recent quantum IC created by the University of Bristol, where the photon manipulation is reprogrammable.
 
Cabe
http://twitter.com/Cabe_e14
  • Sign in to reply
Parents
  • DAB
    DAB over 14 years ago

    I worked on some interferometer fringe analysis devices back in the 1980's.  If they have improved the optics and combined them with new image processing algoritims, these devices could yeild some very interesting devices.

    I can see a lot of the technology that was not available then, coming to fruition in recent years.  They might actually begin to get optical computing devices practical enough to use.

     

    Definitely need to keep an eye on this research.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Catwell
    Catwell over 14 years ago in reply to DAB

    Dab,

     

    Every consider consulting in the quantum research department? That is, if you have extensive experience with the tech.

     

    Cabe

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 14 years ago in reply to Catwell

    An interesting idea, but as I stated, my knowledge is a few decades old.  I am sure there are many new photonic engineers who are much more in tune with the current technology.

     

    While I probably could not help much, I can see many potentials for the technology based upon some of the programs I used to work on.

    Like I posted earlier, keep an eye on this one.  It could soon get interesting.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 14 years ago in reply to Catwell

    An interesting idea, but as I stated, my knowledge is a few decades old.  I am sure there are many new photonic engineers who are much more in tune with the current technology.

     

    While I probably could not help much, I can see many potentials for the technology based upon some of the programs I used to work on.

    Like I posted earlier, keep an eye on this one.  It could soon get interesting.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
No Data