Publications
  • Learn
  • More
Publications
Blog All-Carbon Near-Infrared PV Cell
  • Blog
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Publications to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 2 Jul 2012 7:01 PM Date Created
  • Views 799 views
  • Likes 1 like
  • Comments 2 comments
  • research
  • alternative_energy
  • mit
  • industry
  • on_campus
  • cabeatwell
  • prototyping
  • measurement
  • university
  • energy
  • solar
  • solar_cell
  • sensor
  • innovation
Related
Recommended

All-Carbon Near-Infrared PV Cell

Catwell
Catwell
2 Jul 2012

image

Single-wall carbon nanotube coated silicon surface. Imaged with a atomic-force microscope. (via MIT & Rishabh Jain)

 

Carbon not only provides the foundation for all living things on earth, but it can create some of the most useful materials like carbon fiber and graphene. It can even smell rotting fruit. Now, carbon nanotubes are expanding the range of light rays that can be harvested from the sun. Conventional PV cells harvest photons in the visible spectrum, but researchers at MIT have found out how to manufacture a PV cell exclusively out of carbon nanotubes and C60 (buckyballs) to capture near-infrared energy. 

 

 

A team led by chemical engineering professor Michael Strano, is working with Italian company Eni, to create the first all-carbon PV cell that does not need polymer layers. Near-infrared photons make up 40% of the solar energy from the sun, and this reserve is what the carbon nanotube cells will collect.

 

 

Initial tests have proven the concept of the all-carbon cell but have only provided a 0.1% energy conversion efficiency so far. However, the layer of carbon nanotubes is so thin, the PV cell is transparent and could be used in conjunction with conventional cells to take advantage of a wider photon spectrum. As far as the team can tell, their cell is stable in air, which distinguishes it from previous carbon cells.

 

 

The project has already revealed what works, what does not and how the prototype can be improved. They found that a heterogeneous mixture of different types of carbon nanotubes does not work. Instead, researchers hope to improve the efficiency of the cells by experimenting with the exact shape and thickness of the layer of very pure, uniform, single-walled nanotubes.

 

 

Because of the nanotube’s exceptionally high light absorption, these all-carbon PV cells require relatively small amounts of carbon and are extremely lightweight. Keeping the cost low, even at a low efficiency, makes these infrared PV cells enticing and worth refining.

 

 

The research is supported by the NSF and fellowships from the U.S. DoD.

 

Cabe

http://twitter.com/Cabe_e14

  • Sign in to reply
  • Catwell
    Catwell over 13 years ago in reply to DAB

    Energy is always needed, I think they should release what they have. It is on par with some of the older generations of solar cells. Through production they can gain funding, more research, etc..

     

    Cabe

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 13 years ago

    Interesting, but there is a lot of productization that needs to happen before we see them on a roof near you.

     

    It looks like this approach has potential, but there a lot of unknowns I would like to see answered, like efficiency, power and heat transfer, connectivity issues, durability, etc.

     

    Good promise thought,

    DAB