Publications
  • Learn
  • More
Publications
Blog Alternative to uranium, here all along
  • Blog
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Publications to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Eavesdropper
  • Date Created: 20 Jun 2011 11:13 PM Date Created
  • Views 1024 views
  • Likes 1 like
  • Comments 6 comments
  • research
  • alternative_energy
  • nuclear
  • dit
  • eavesdropper:dit
  • university
  • energy
  • innovation
Related
Recommended

Alternative to uranium, here all along

Eavesdropper
Eavesdropper
20 Jun 2011
image
EMMA ring and ERLP accelerator (via Daresbury & Wikipedia)
 
In the wake of the Fukushima disaster, many have been searching harder for an alternative to Uranium based nuclear energy generation. Alternative thinking, as a majority, was put aside in the effort to develop technology that could work alongside of, and benefit from research pertaining to, nuclear weapons. Research at UK's Daresbury science park have brought back an old alternative to uranium, thorium.
 
Thorium, discovered in 1828, has long been known to potentially have the same energy producing qualities as uranium. In 1996, the International Atomic Energy Agency began a study over the use of thorium reactors. Some of the benefits show it to be a clear winner over uranium or plutonium. Thorium produces 10 to 10,000 times less radioactive waste. The thorium used in the fission reactors come out of the earth in the state needed for usage. It is difficult to pull weapons-grade materials from a thorium reactor. And the nuclear chain reaction in thorium requires priming, and the reaction stops if the energy introduced stops. In other words, thorium will never produce a meltdown. Finally, the thorium supply is much more abundant that uranium. The study found that the raw supply will not be exhausted, in used as an energy source, for 1,000 years.
 
At Daresbury recently, the EMMA (Electron Machine with Many Applications) particle accelerator was show to be able to produce the energy needed to foster the chain reaction in thorium. Such facilities, and energy needed, does make the use of thorium much more expensive than reactors today. Along with the study on thorium, the Britain team at Daresbury are also researching the use of particle accelerators to treat hard to reach cancer in patients.
 
Sound like they are doing some fine work across the pond.
 
Eavesdropper
 
Thorium fun facts: The name is derived from Thor, the Norse god of thunder. Attomic number 90, it has 90 protons and electrons. 4 are valence electrons. It is a solid, white like metal.
  • Sign in to reply

Top Comments

  • DAB
    DAB over 14 years ago +1
    For those of you too young to remember vacuum tubes, Thorium was used to initiate the electron cloud around the cathode so that the grid voltage could control the number of electrons that went to the anode…
  • billpenner
    billpenner over 14 years ago in reply to Former Member

    Do you know the purpose of Thorium in the mantles? I have been around electronics for many years and knew about Thorium and its purpose in vacuum tubes but was not aware of its use in mantles, although they were the only lights we had in tents while hunting in the mountains of New Mexico..

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • yogi1940
    yogi1940 over 14 years ago in reply to DAB

    AS you say DAB, very well stated I also entered electronics studing and using vacuum tubes. I well remember some great experiments we got up to. Lots of dirty brown smells.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Eavesdropper
    Eavesdropper over 14 years ago in reply to Former Member

    Keep in mind, thorium is still radioactive. Not as much as current  nuclear fuels, but still up there. However, that is a good idea.

     

    More  research in thorium needs to happen. Luckily, India is building a  thorium heavy water reactor, and is scheduled to go into operation some  time this year, 2011. 300 MW is the output, but it uses a plutonium core  to start the reaction, not an accelerator.

    Hopefully, installations like this will help push thoriums adoption.

     

    E

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Former Member
    Former Member over 14 years ago

    Thorium is also a component of mantles used in gas powered camping lanterns and outdoor lights. At one time it was necessary to placard shipments of Coleman mantles as radioactive.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Syster
    Syster over 14 years ago

    As a Canadian, I was shocked to discover that the CANDU reactors were originally designed to use Thorium, but were switched over to Uranium for political purposes.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
>