Publications
  • Learn
  • More
Publications
Blog An algorithm to charge batteries faster than even, $4 million to develop
  • Blog
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Publications to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 10 Oct 2012 6:22 PM Date Created
  • Views 693 views
  • Likes 0 likes
  • Comments 2 comments
  • research
  • alternative_energy
  • industry
  • battery_charge
  • on_campus
  • lithium_ion
  • Design
  • battery
  • cabeatwell
  • prototyping
  • university
  • energy
  • energy_storage
  • innovation
Related
Recommended

An algorithm to charge batteries faster than even, $4 million to develop

Catwell
Catwell
10 Oct 2012

image

Dramatic shot of the researchers researching. Professor Miroslav Krstic at left, and Postdoctoral Scott Moura on the right are the leads in the project (via University of California)

 

 

Sometimes scientists and engineers oversee problems with conventional methods, leading to scrapped projects when these conventions are not questioned. An example of this is the cancellation of the Toyota eQ electric vehicle due to Toyota’s lack of confidence in how consumers view EVs, mostly in the area of battery charging times. This traditional take may soon change.

 

 

A research team at the Jacobs School of Engineering at UC Davis, has received a $4 million dollar grant from the DOE’s ARPA-E to develop and test mathematical models and battery operating algorithms that will make more effective and efficient use of lithium ion batteries. Lowering their size, cost and charging times while increasing longevity is the focus for the group. These tests will be done in conjunction with electric vehicle equipment from the automotive firm Bosch and battery manufacturer Cobasys, whom received most of the grant.

 

 

The vast majority of conventional battery monitoring methods simply look at the voltage across the battery and resulting current to indirectly infer information like charge and the battery operating condition. Postdoctoral Fellow Scott Moura, said this method is like trying to figure out how fast and where people sat in a theater, simply by looking at how fast the line moves. The team is hoping that mathematical models can provide a better understanding of where “people are sitting” so that “broken seats” can be identified and the theater can be filled to its maximum efficiently and safely. Bringing this analogy back to the original conversation of batteries, the team hopes to refine estimation mathematical models that will describe the distribution of Li+ ions throughout the battery. This would allow for better gauging of battery longevity as well as identify damaged sections. That information will also lead to finding optimum charging rates and times, so that Li-ion batteries can be discharged and charged at their maximum efficiency safely.

 

 

Once the algorithms and mathematical models are refined, the team expects the cost of manufacturing Li-ion batteries could be decrease by 25% as they can be smaller, used more efficiently and have increased longevity. This could also result in batteries charging in half the time of today’s batteries. In one instance (though it is unclear which instance is being referred to) the UC-Davis team said charging time could be as fast as 15 mins. Elegance over brute force is always preferred.

 

 

Cabe

http://twitter.com/Cabe_e14

  • Sign in to reply
  • awneil
    awneil over 13 years ago

    I don't think it's true to say that, "conventional battery monitoring methods simply look at the voltage across the battery"?

     

    I think there are techniques such as modulating the load current to gain better information?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 13 years ago

    I am not sure that you will get much return on your investment for this project.

    The current methods may not be ideal, but they are simple and easy to implement.

    I am doubtful that you can come up with a single solution because of the vast differences in the battery chemistry.

     

    To make this approach work, you would need an extremely stable battery with zero differences in the production facility.  Not too likely to my mind.  Plus, what we talking about, a few watts per battery?

     

    I think they should look at more reversable battery configurations.  The best you can hope for is a fully rechargable system with little or no degredation with time.  Maybe a sealled H20 system.

     

    Just my opinion,

    DAB