Publications
  • Learn
  • More
Publications
Blog Arduino in a production device, the camera Triggertrap
  • Blog
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Publications to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Eavesdropper
  • Date Created: 6 Dec 2011 8:56 PM Date Created
  • Views 842 views
  • Likes 1 like
  • Comments 1 comment
  • time_lapse
  • photography
  • triggertrap
  • embedded
  • eavesdropper
  • camera
  • electronic_products
  • arduino
  • innovation
Related
Recommended

Arduino in a production device, the camera Triggertrap

Eavesdropper
Eavesdropper
6 Dec 2011
You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 
I lost a bet. The wager was against anyone selling an Arduino device for any purpose besides one-of-a-kind projects or development.
 
Along came the "Triggertrap." An Arduino based universal camera trigger. The system has onboard contectivity for wired and wireless camera connections. There is a 2.5mm mini-jack for wired, IR for wireless. Onboard light and sound sensors can be used to trip the camera. (Snap a flash anywhere, and the camera will go off.) An auxiliary jack allows the Triggertrap to be activated (or activate) anything capable of generating a signal. USB is also available for power or software updates. Production has started, and should be available in February. Standalone version is $125 and an Arduino shield with the same features is $75. Up to 144 cameras are already supported.
 
The camera aficionados out there, the Triggertrap can also be used and a slave flash device. Multiple cameras can also be tripped. Most useful, in my opinion, is the time-lapse function. Set the interval, and let the fun begin.
 
image
Dual camera triggering (via Triggertrap)
 
I am also posting about this project as an example how taking what one already knows and developing it into a viable, now popular, product.
 
Eavesdropper
  • Sign in to reply
Parents
  • DAB
    DAB over 14 years ago

    I have been seeing different designs for this device for a couple of years now.  What I really need is a device that can trigger a regular digital camera under computer control.  The DSLR's have the capability, but all digital cameras should be equiped for this capability.  All it would take is some software to the USB port and we could do a lot more with the cameras than just take pictures.  I need several to collect specific image data at specific events.  I am not sure this one will solve my problem, but I will keep an eye on it as it comes to market.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 14 years ago

    I have been seeing different designs for this device for a couple of years now.  What I really need is a device that can trigger a regular digital camera under computer control.  The DSLR's have the capability, but all digital cameras should be equiped for this capability.  All it would take is some software to the USB port and we could do a lot more with the cameras than just take pictures.  I need several to collect specific image data at specific events.  I am not sure this one will solve my problem, but I will keep an eye on it as it comes to market.

     

    DAB