Publications
  • Learn
  • More
Publications
Blog Are hexapod CNC milling machines fazing-out conventional mills?
  • Blog
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Publications to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 17 Sep 2012 6:48 PM Date Created
  • Views 3100 views
  • Likes 2 likes
  • Comments 6 comments
  • research
  • industrial
  • industry
  • hmi
  • manufacturing
  • robotics
  • robot
  • chicago
  • machines
  • cabeatwell
  • prototyping
  • measurement
  • milling
  • tools
  • imst
  • sensor
  • innovation
Related
Recommended

Are hexapod CNC milling machines fazing-out conventional mills?

Catwell
Catwell
17 Sep 2012

image

Tormach PCNC1100 conventional XYZ milling machine (via Tormach)

 

Manufacturing technology becomes more refined to the point where anyone can make complicated parts on the cheap. That was my take at the International Manufacturing Technology Show 2012 in Chicago. This trend not only applies to new product design but updated manufacturing tools such as hexapod milling machines, which seems to be the direction manufacturing is taking. In particular, hexapod actuated machinery had permeated both fabrication of parts and measurement.

 

The question is; are they an improvement over conventional horizontal or vertical CNC mills? Milling machines made their debut around 1829 with the introduction of James Nasmyth’s milling machine which was advanced for its day and could mill the six sides of a hex nut which was mounted in a six-way indexing (moving) fixture that used a flexible shaft made from coiled wire for rotary movement. They have since evolved over time to include computers, which saw the birth of CNC (computer Numerical Control) and CAM (Computer Aided Manufacturing) milling machines. These types of machines made it easy for manufacturers to gain increased precision as well as the ability to move on 3 axis (XYZ) along with horizontal CNC mills that have an additional axis in either C or Q which allows the horizontal work-piece to be rotated (eccentric turning).

 

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image
You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

LinuxCNC EMC2 hexapod (via PKM077)

 

 

Advancements in machine milling haven’t slowed and have once again been transformed incorporating new technology as it becomes available. This includes robotics that enables the mill to achieve a greater range of precision movement such as the LinuzCNC EMC2 hexapod robotic mill. Designed by some hobbyists on the parallelrobots blogspot, the robotic hexagonal CNC mill is situated inside of a boxed metal frame and has a range of motion of 6-DOF (Degrees of Freedom). This is achieved through 6 prismatic actuators (Stewart platform/Parallel robot) positioned at the top of the mills frame. The actuators take advantage of a series of DMM Technology servos, along with 25X10mm ballscrews, to move the actuators along 3 linear movements (XYZ) as well as 3 rotations (pitch, roll and yaw). The ballscrews are connected to a series of cardanic joints that connect to the mills base that connects the mills 2.2kW water-cooled 24,000 RPM spindle. The machine is connected, VIA LPT port, to a computer running Linux-based EMC2 that translates G-code to run CNC mills (as well as lathes, plasma cutters, robots, etc.).

 

The designers of the mill eventually incorporated a MESA 7i43 FPGA-based USB/EPP Anything I/O card to increase the speed and acceleration of the mill. Surprisingly the mill is quite rigid but, as of now, cannot handle machining with steel but that could soon be accomplished in later revisions. So are hexapod CNC milling robots making conventional CNC mills obsolete? The answer is no, not just yet as many home hobbyists have taken to cheap smaller machines (with free source-code for that matter) to use for projects. That doesn’t mean that in the next ten years hexapod CNC mills will not quietly usher-out the technology that’s standard today. As more and more hobbyists are implementing robotic platforms one thing is for sure; eventually conventionalisms falls away as new technology evolves.

 

Cabe

http://twitter.com/Cabe_e14

  • Sign in to reply
  • adamkuk
    adamkuk over 4 years ago

    just useful information:

    The principle of milling is simple: the cutting tool - cutter - carefully and accurately, layer by layer, removes everything unnecessary from the surface of the workpiece.

    The benefit:
    - Quality brings money.
    - Features without borders
    - Areas of use


    Quality brings money
    What is the first thing you look for when you go to the stores? Right, the quality of the product.

    And you want to be the best in your business too, making quality the top priority.

    A cnc router machine will increase the profits of any metal or non-metal processing business because:

    - Precision and speed of cutting
    - Minimal rejects and waste
    - Three-dimensional image creation
    - High productivity
    - Fast payback
    - No carbon build up and no burrs
    - Automation in production
    All of the above advantages can be summarized in one concept - quality. With quality you can always win.

    Possibilities without borders
    The popularity of the milling machine did not arise out of nothing.

    Can you imagine the production perspectives that are opened up by this high-tech equipment? With what materials and how can work these toothy masters - cutters?

    Materials to work with:
    - Wood
    - Acrylic
    - Plywood
    - Plexiglass
    - Soft metals
    - PVC, MDF and chipboard
    - Polystyrene and PET
    - Model plastic
    - Stone, granite, marble
    For example, for milling large planes often choose end mills and cylindrical cutters, angular cutters are ideal for obtaining grooves, undercutting, the processing of inclined surfaces and angular grooves.

    Roughing and finishing hobbing is carried out by a hobbing cutter. The shaping cutter is used for profile machining.

    Applications
    The list is huge and can be continued, so the choice of tool modification of the machine tool for milling depends on the tasks set and the application.

    Molds
    - Technology tooling.
    - Props for photographic studios and theaters.
    - Souvenir production.
    - Decorative elements of an interior.
    - Furniture manufacture.
    - Electrical engineering and electronics.
    - Advertising and POS materials.
    - Example of work on the cutter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago

    Great and informative piece. What about installing a retrofit kit to keep your mill current as the years go on? http://www.cncmasters.com/blog/how-can-a-retrofit-kit-change-your-business.html

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago

    The cnc industry has change a lot in the last years, prices are getting low for the flat cnc machines make in it possible to small machinist to have a cnc mill. The Hexapod is a nice improve making possible to produce different type of outcome or pieces.

     

    Torno cnc

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago

    Grate post! Good topic thank you for sharing this information. CNC milling machine is used to machine solid materials. There is two basic forms of it. Milling machine can perform a vast number of operation, from simple to complex.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Catwell
    Catwell over 13 years ago in reply to DAB

    Small businesses in the USA need the ability to fabricate using 6 axis, inexpensively. A feb tech that has been exclusive to the higher end shops. As development progresses, I hope to see cheaper CNC gear for the masses.

    I even think that the cheapest 3D printer needs to come down a bit too.

     

    Cabe

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
>