Publications
  • Learn
  • More
Publications
Blog ARM releases new scalable GPU for entry and midrange mobile devices
  • Blog
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Publications to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 21 Jun 2012 4:18 PM Date Created
  • Views 687 views
  • Likes 2 likes
  • Comments 2 comments
  • research
  • ic
  • industry
  • processing
  • cell_phone
  • multi_core
  • embedded
  • mobile
  • cabeatwell
  • prototyping
  • gpu
  • cpu
  • arm
  • innovation
  • communication
Related
Recommended

ARM releases new scalable GPU for entry and midrange mobile devices

Catwell
Catwell
21 Jun 2012

image

Mali core concept (via ARM)

 

As mobile devices increase in popularity, demand for silicon-based processing power rises. This includes GPUs, without which we could not game, watch HD movies and alter photography. All of which are extremely necessary in this day and age of social-site based communications with others (that’s technical jargon for hooking up with friends on Facebook, Twitter, etc), retaining high-score positions on Angry Birds and sharing recent pic’s with location mapping on Four Square. To that end most of that processing power comes from companies such as ARM who recently released their new GPU, named Mali-450MP, to help scale well with existing and future CPUs in the mobile device market.

 

This means that companies such as HTC, Nokia and LG can extend the use of their current software platforms, as well as future platforms, using ARM’s new Mali-450 series GPUs Graphical Processing Unit). It also provides an increase in support of up to 8 CPU cores over its predecessor the Mali-400 which can only support 4 cores, which means the 450 can pump-out an increase in pixel processing and vertex shading throughput. Simply put, better visuals for games, pictures and videos for entry level and mid-range mobile devices.

 

So, what’s packed onto the new 8.6mm2 die? How about 4 processing cores with 256k of level 2 cache with each core running at 240MHz (in LP mode) or 480MHz (in GP mode) respectively. Running at 480 MHz provides 104M triangles with 3.8G pixels running with 4 X FSAA (Full-Screen Anti-Aliasing) with support for OpenGL 1.1/2.0 which is pretty impressive. The ARM Mali-450MP is available now for OEM manufacturers (price unknown at this time).

 

Cabe

http://twitter.com/Cabe_e14

  • Sign in to reply
Parents
  • DAB
    DAB over 13 years ago

    I would consider this part to be among the first where you begin integrating multiple CPU's with memory and data passing integrated into a single package.  While I suspect that only a handful of people can really exploit the power, that will change over time as new ways of parallel and distributed processing evolve.

     

    The future is changing in computing.

     

    Just my opinion,

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 13 years ago

    I would consider this part to be among the first where you begin integrating multiple CPU's with memory and data passing integrated into a single package.  While I suspect that only a handful of people can really exploit the power, that will change over time as new ways of parallel and distributed processing evolve.

     

    The future is changing in computing.

     

    Just my opinion,

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • Catwell
    Catwell over 13 years ago in reply to DAB

    All-in-one-chip is the true goal.

     

    Cabe