Publications
  • Learn
  • More
Publications
Blog Atmel shows new maXTouch S series chip at CES 2012
  • Blog
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Publications to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 13 Jan 2012 6:32 PM Date Created
  • Views 557 views
  • Likes 0 likes
  • Comments 1 comment
  • touch
  • hmi
  • cell_phone
  • microcontrollers
  • embedded
  • Design
  • cabeatwell
  • ces
  • touchscreen
  • ces2012
  • innovation
  • atmel
Related
Recommended

Atmel shows new maXTouch S series chip at CES 2012

Catwell
Catwell
13 Jan 2012
image
Panel concepts by Atmel @ CES 2012
 
All-in-one micro-chips are the unseen heroes in today’s electronics, and the announcement of Atmel’s new maXTouch S Series Touchscreen controllers are sure to go unsung into widespread adoption. The first, of three, is designated as mXT224S and has a 224-node controller that can handle cameras, smartphones and other devices that incorporates a touchscreen size of up to 4.3 inches. The next in line is the mXT336S which features 336-node controller for screens measuring up to 5.5 inches on the diagonal. This chip could be used to power screens for smaller tablets or bigger phones and next-gen hand-held gaming consoles. The third chip in this roundup is the mXT1664S which is for screens measuring up to an astounding 17 inches, full-size tablets.
 
The chips also passed Microsoft’s strict guidelines for integration with Windows 8 making them more appealing to companies who are designing new products centralized around the upcoming OS.  All chips feature Atmel’s SlimSensor Technology which helps to control ‘display noise’ associated with high-res or HD displays through a combination of hardware and firmware. Another feature all the S series chips use is Atmel’s ‘maXStylus’ which enables multi-touch pressure sensing for both fingers and stylus writing implements. The maXTouch S Series Touchscreen controllers are now available for sampling for mobile developers with full production chips coming in Q1 of this year.
 
Cabe
Follow my CES walk at:
http://twitter.com/Cabe_e14
  • Sign in to reply
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    Unseen, but  thanks to engineer reporters at CES, not unsung. Thanks for the report. The mXT1664S is truly astounding.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • e14 Contributor
    e14 Contributor over 14 years ago

    Unseen, but  thanks to engineer reporters at CES, not unsung. Thanks for the report. The mXT1664S is truly astounding.