Publications
  • Learn
  • More
Publications
Blog Autonomous robot plays catch
  • Blog
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Publications to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Eavesdropper
  • Date Created: 3 May 2011 2:20 AM Date Created
  • Views 499 views
  • Likes 0 likes
  • Comments 0 comments
  • research
  • test
  • dit
  • eavesdropper:dit
  • hmi
  • robotics
  • robot
  • measurement
  • innovation
Related
Recommended

Autonomous robot plays catch

Eavesdropper
Eavesdropper
3 May 2011
You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 
The German Aerospace Agency, DLR, has release a mobile robot platform with a humanoid upper body with two arms and a head, called the "Rollin' Justin." For the time being, they are testing and working on improving the accuracy of catching a ball (or 2) and working with everyday items and tasks. Each hand has 4 fingers and a slew of sensors, allowing it to firmly or gently interact with objects. The head consists of two stereo cameras and a PMD sensor. The head acts like a more advanced Microsoft Kinect, allowing for 3D mapping of the environment. For use interaction, and configuring, an iPad based application is available.
 
The overall catch accuracy of the Rollin' Justin is approximately 80% at the moment. It can move its hand within 2cm of actual balls position, but it can move it there in a frightening fast 5 milliseconds. Although the camera sensors are accurate, it can not see its own fingers clearly. It relies on tactile feedback as it operates the coffee machine in the second part of the first video. Improving the image recognition is the  essential next step for DLR. Then their "Household Robot" may very well be just that.
 
Eavesdropper
 
This bot is reminiscent of the character Johnny 5 of the film "Short Circuit." Except here, it operates autonomously. Johnny 5 was more like a puppet, the operator wore an exoskeleton like suit to operate that guy.