Publications
  • Learn
  • More
Publications
Blog Carbon Nanotubes Can “Smell” Rotting Produce
  • Blog
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Publications to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 3 May 2012 6:14 PM Date Created
  • Views 1344 views
  • Likes 1 like
  • Comments 1 comment
  • research
  • industry
  • hmi
  • on_campus
  • Design
  • cabeatwell
  • prototyping
  • carbon_nanotube
  • measurement
  • university
  • medical
  • sensor
  • innovation
  • communication
Related
Recommended

Carbon Nanotubes Can “Smell” Rotting Produce

Catwell
Catwell
3 May 2012

image

Concept of the sensor (via MIT & Wiley Online Library)

 

The list of applications for carbon nanotubes seems to keep growing and growing. Scientists at MIT have found a way to give these nanotubes the capability of detecting gasses that are present during the process of ripening and rotting of fruits and vegetables.

 

 

These sensors consist of tens of thousands of carbon nanotubes that have been treated with copper atoms and polystyrene. Ethylene, a gas present during the ripening process, sticks to the copper and thus slows the flow of electrons through the carbon nanotubes. The higher the ethylene content in the air, the slower the electron flow is, and this can be correlated to determine the stage of ripening or rotting. Combining the sensor with an RFID chip allows for real time monitoring of produce. The sensor detects 0.5 parts per billion of ethylene in the air which makes it extremely sensitive. The sensor itself can be manufactured for only 25 cents, while the addition of an RFID chip increased the price to only $1 total per unit.

 

 

These sensors could change how produce is handled in stores like when it is put on clearance. This sensor can also be used to manage plants in new and beneficial ways. According to the USDA, 10% of produce is lost to spoilage annually.

 

 

The U.S. Army Office of Research funded the MIT research. The army is hoping this paves the way to more general electrochemical sensors such as mold or bacteria detectors.

 

Cabe

http://twitter.com/Cabe_e14

 

A brief collection of Carbon Nano-tube related news:

The 9 nanometer carbon nanotube transistor

First flexible carbon nanotube logic circuit printed

Graphene made cheap and green

Liquid smoke reformulated for new energy storage use

5 times the density in ICs

Biological enhancement to solar cells

Sensor detects one molecule of explosive

New scale able to weigh the light-weighted while you wait; the single atom scale

Carbon-nanotube based Ink-jet printer on the way

Wireless printed sensor detects explosives at a distance

Stretchable nanotube transistor material from DOE Berkely, a touch interface

  • Sign in to reply
  • DAB
    DAB over 14 years ago

    Another great research discovery, but I still want to know "when" we will see actual devices available using nanotubes for enhanced sensing.

     

    I agree that the potential looks awesome, but then I thought magnetic bubble memory would be a big deal also.

     

    Time will tell.

     

    DAB