Publications
  • Learn
  • More
Publications
Blog CES 2013 Extreme Reality's 2D camera system - any webcam can operated like a 3D tracker
  • Blog
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Publications to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 11 Jan 2013 7:29 AM Date Created
  • Views 530 views
  • Likes 1 like
  • Comments 2 comments
  • research
  • transportation
  • 3d
  • hmi
  • 2d
  • embedded
  • motion_capture
  • cabeatwell
  • prototyping
  • measurement
  • extreme_reality
  • kinect
  • sensor
  • innovation
  • communication
Related
Recommended

CES 2013 Extreme Reality's 2D camera system - any webcam can operated like a 3D tracker

Catwell
Catwell
11 Jan 2013

image

Extreme Reality's "Extreme Motion" concept art. Captures 3D motion from a 2D camera. (Via Extremem Reality)

 

The world of 2D webcams just picked up another dimension. The company responsible, Extreme Reality, is showing off their new software that converts images from any plug-in or built-in webcam into a 3D motion tracker at CES. The company says its software will reproduce the same accuracy or better compared to expensive 3D cameras with depth sensors. Not only can you save cash using inexpensive webcams for gesture tracking, but you can program your own games using the platform, which can be accessed for free if the company accepts your request for development.

 

 

The Extreme Motion platform can be used to program 3D motion tracking to any Android or iOS device. The company has developed a racing game, a dance game and virtual tennis that demonstrate Extreme Motion’s abilities. The platform can be adapted to work on TVs, PCs, smart phones or tablets; pretty much anything with a video camera.

 

 

Extreme Reality also offers something called the Extreme UI. This interface allows the user to use pre-programmed gestures to control a PC. The user can drag and drop items, open and close programs and swipe through web pages by natural, intuitive gestures. Users can also customize and define new gestures for specific applications. This interface can also replace your mouse by allowing you to perform all its functions with your hands.

 

 

For an idea of system requirements needed to run Extreme Motion, their PandaMania game (dancing) works on an Intel core i5 1.5GHz and is compatible with any standard camera with minimum of 640/480 VGA resolution (same res as the Kinect's RGB and IR cameras. I wonder if this system could work with Kinect for Windows - better or worse?). This game currently runs only on Samsung devices using Windows 7 or Windows 8.

 

 

The system works well registering body motions up to 17 ft away (5 m). The program calculates the position of all joints every frame so error is corrected immediately and motion is represented seamlessly in real time. It is not sensitive enough to register finger motion at this range but with time and more developers improving upon it, it will surely get better.

 

Now for an overt - overview...

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Cabe

http://twitter.com/Cabe_e14

  • Sign in to reply
Parents
  • DAB
    DAB over 13 years ago

    I like the approach here, though I am surprised that it took someone this long to workout the details.

     

    You have several freeware projects going for years that worked out the 2D to 3D translations and the software to map 2D images into three space has been around for decades.

     

    As the video shows, there are now few impediments to allowing a person to embed themselves into a virtual world and interact with real and imaginary players.

     

    My only question is where do the gaming folks go next?

     

    Just my opinion,

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Catwell
    Catwell over 13 years ago in reply to DAB

    Improve the motion tracking and go into a virtual reality in 3D space.

     

    The new XBOX, due out at the end of 2013, is rumoured to project images all around a 3D space. I look forward to seeing that in action.

     

    C

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Catwell
    Catwell over 13 years ago in reply to DAB

    Improve the motion tracking and go into a virtual reality in 3D space.

     

    The new XBOX, due out at the end of 2013, is rumoured to project images all around a 3D space. I look forward to seeing that in action.

     

    C