Publications
  • Learn
  • More
Publications
Blog Communications Interoperability in a Disaster
  • Blog
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Publications to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: gervasi
  • Date Created: 11 Sep 2011 7:28 PM Date Created
  • Views 681 views
  • Likes 1 like
  • Comments 1 comment
  • communications
  • cgervasi:dit
Related
Recommended

Communications Interoperability in a Disaster

gervasi
gervasi
11 Sep 2011

Lately I have come across articles about Congressional measures to improve public safety communication interoperability in the event of a disaster like the Sept 11 attacks.  The narrative goes that the 9/11 Commission recommended public safety radio equipment be made interoperable so members of different police and fire departments could communicate with one another, and this plan is simply implementing the recommendations.

 

The legislation would auction two 5 MHz segments of spectrum in the 700MHz range (formerly used by UHF TV channels 62 and 67) to non-emergency users with the understanding they would not use those frequencies in an emergency.  The auction proceeds would be used to pay for an interoperable radio system that would support dozens of duplex pairs of voice channels, data transfer, and streaming video.

 

Some articles frame this issue as allocating 10MHz of spectrum to the cause of interoperability.  Supporters were hoping to pass the bills before the tenth anniversary of the September 11 to capitalize on an increased focus on disaster preparedness.

 

imageHow will 10MHz of spectrum be used for interoperability?
It won’t.  It will allow more streaming data and more users on a single repeater.  The new spectrum is located adjacent to two 5 MHz segments (formerly used by UHF channels 63 and 68) currently allocated to public safety.  This would allow single transmissions with a bandwidth greater than 5 MHz.

 

When you dig into supporters’ arguments, they say public safety needs the additional bandwidth to support higher data throughput, not for interoperability.

 

How much spectrum bandwidth does it take to get a given amount of data throughput?
Bandwidth and data throughput are related so closely that the term “bandwidth” is sometimes used colloquially to refer to data throughput.  The theoretical throughput capacity of a channel is defined by Shannon’s Law: C = B log[2] (1+S/N), where C is throughput capacity and B is the channel bandwidth.  If you have enough signal to noise ratio, you can get any throughput you want even on a small amount of bandwidth.  In a practical system, limitations of the dynamic range of the receiver, interference from other radio systems, interference from reflections off various objections in the environment, and the Gaussian noise in the receiver’s components all limit the maximum signal to noise ratio.  It works out that in a practical system deployed in the field, you can get a maximum of 1 Mbps per every 1 MHz of spectrum space.  In marginal channel conditions, you may get a tenth of that.  This means you can fit one streaming video channel into 1 MHz of spectrum.

 

How should interoperability be accomplished?
Emergency repeaters could be set up that have one input frequency and one output frequency in each band allocated to public safety.  All inputs would be re-transmitted on all outputs.

 

The reason for multiple inputs would be to allow each agency to program that frequency into their existing radios without buying new equipment.  There should also be a simplex frequency so in the event of failure or loss of contact with any centralized repeater, responders using the same band could communicate.  This approach is almost free.  It also has the advantage of being simple and therefor less prone to failure.  Some local police and fire departments police and fire departments have already worked out interoperability plans like this.

 

The proposed system is the opposite of a quick-and-dirty approach.  It appears to be a way to find $6 to $10 billion for public safety agencies to buy some very nice equipment from companies like Motorola.  I am not knowledgeable about how useful high-end communications equipment is to responders in an emergency situation.  If it’s reasonably useful, we should spend the money instead of trying to find a cheap solution.

 

It is unfortunate that the Sept 11 attacks have been invoked so often to prop up dubious arguments.  It usually requires aggrandizing the perpetrators of the crimes and belittling the power of democratic societies operating under the rule of law.

 

Supporters of the proposed interoperable broadband system need to make separate cases for why they need more bandwidth and more equipment.  I like advanced radio equipment, so I would love to hear the amazing things it can do.  I condemn evoking Sept 11 as the reason for new equipment and more bandwidth, but I am open to cogent arguments on the merits vs. costs.

 

Does public safety need $10 billion and/or 10MHz more to communicate in a disaster?

  • Sign in to reply
  • DAB
    DAB over 14 years ago

    Thanks for pointing out one more Government Boon Doggle.  I agree that public safety is important, but as you point out, this is another gold plated solution that is unproven to work during emergency situations.

    Having survived a few "emergencies" I have observed that a handful of volunteers using CB radios are a whole lot more effective than a lot of these fancy radio systems.  Yes I know that the CB is not a secure radio, but in an emergency, the speed at which the information can be transferred is much more important than who else knows it.

    When you look at most of these systems, the big problem is where they are installed.  As they found in New York, when your emergency management office is the site of the emergency, you are left without an adequate response capability.

    To deal effectively with emergencies, you need a solid but simple process with a minimum of procedures and a staff trained to implement the process instantly.  All of the technical toys do not accomplish this need.

    I have seen many of these expensive and fancy solutions to simple problems.  They all fail because the users are lured into a false sense of security because of the technical capabilities of their devices.  They forget that if the people are not fully trained to exploit those capabilities, then you still end up with chaos.

    In my experience, you want to go simple early and often.  Knowing what to do is a whole lot more important than having a device that is too complicated to use when people are stunned or overly excited.  If you have trained people throughout the area who can organize the many volunteers who emerge from the survivors, you can do a much better job than trying to play mother may I with distant and clueless managers.

     

    Just my observation.

    DAB