• Products and Partners
    Products and Partners
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
Publications
  • Learn
  • More
Publications
Blog DARPA Initiative Seeks Affordable Wafer-scale Infrared Sensors and Cameras
  • Blog
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Publications to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: GardenState
  • Date Created: 18 Sep 2015 12:56 AM Date Created
  • Views 1279 views
  • Likes 0 likes
  • Comments 1 comment
  • us_defense
  • infrared_sensor
  • wired
  • darpa
Related
Recommended

DARPA Initiative Seeks Affordable Wafer-scale Infrared Sensors and Cameras

GardenState
GardenState
18 Sep 2015

image

The low cost of digital imaging devices has allowed them to become popular consumer products.  This low cost is made possible by leveraging a mature processing infrastructure and the ability to fabricate complete focal plane arrays (FPAs) at the wafer scale.  A similar trend is occurring on a smaller scale with thermal imaging technologies.  Microbolometers that are sensitive in the long wave infrared (LWIR) spectrum and are used as a detector in a thermal camera are also manufactured at the wafer scale, and the resulting cost reduction is enabling thermal imagers at consumer‐grade price points.  In contrast, FPAs that respond in the short‐wave and mid‐wave infrared (SWIR and MWIR) spectral bands are currently manufactured using complex and time‐consuming methods that typically involve several manual fabrication steps, including single‐die processes.  Further contributing to high cost is the requirement that MWIR FPAs operate at temperatures < 200 degrees K to achieve good signal‐to‐noise ratios, which requires the use of a cryogenic cooler.

 

Through its Wafer Scale Infrared Detectors (WIRED) program, the U.S. Defense Advanced Research Projects Agency (DARPA) is asking industry to develop infrared sensors and cameras for low-cost, large-format, and high-performance imaging in the SWIR, MWIR and long-wave infrared (LWIR) spectral bands. They are doing so via a broad-agency announcement, designated DARPA-BAA-15-57.

 

Specifically of interest are infrared detector materials that can be monolithically processed on traditional readout integrated circuit (ROIC) substrates at the wafer scale. To minimize cost, size, weight and power (SWaP), MWIR FPA detectors must be able to operate at temperatures above 230 degrees K.

 

DARPA anticipates that through use of current state-of-the-art technology substantial reductions in pixel pitch should be achieved for the same imager format. The program also seeks a better understanding of the fundamental properties, limitations, and benefits of wafer‐scale detector technology.  Finally, WIRED seeks to develop innovative detector technologies in the LWIR spectral band that will enable FPAs to operate without cooling. 

 

Proposals should have as a goal demonstrating prototype SWIR, MWIR, and LWIR cameras that can be field tested. The DARPA WIRED program is estimated to be worth as much as $40 million, with several contract awards expected. Interested organizations should submit abstracts no later than Oct. 9, 2015, and full proposals no later than Nov. 23, 2015 to the DARPA BAA website.

  • Sign in to reply
  • DAB
    DAB over 11 years ago

    The development of good IR sensors have been a huge problem for the last four decades.

    There are so many uses of good IR imaging and yet there have been very few production improvements, which I find totally disappointing.

     

    Granted, the materials needed are not readily available, but they are abundant enough to be affordable.

     

    I think part of the problem has been the manufacturing limitations in working with anything beyond silicon wafers.

     

    Hopefully the rapidly growing Graphene research will reach a level where it can support the development of simple IR sensors.

     

    DAB