Publications
  • Learn
  • More
Publications
Blog Doctoral student looks to power the future with ‘solar hydrogen’
  • Blog
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Publications to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 9 Apr 2012 5:13 PM Date Created
  • Views 653 views
  • Likes 1 like
  • Comments 1 comment
  • research
  • alternative_energy
  • hydrogen
  • industry
  • hmi
  • on_campus
  • Design
  • cabeatwell
  • prototyping
  • university
  • energy
  • solar
  • sensor
  • innovation
Related
Recommended

Doctoral student looks to power the future with ‘solar hydrogen’

Catwell
Catwell
9 Apr 2012

image

(Left) Erik Koepf (Right) Professor Ajay Prasad standing over the solar reactor

 

Using hydrogen refined from natural gas for use as a power source has a fundamental flaw, the process of extraction produces carbon dioxide. This isn’t good for the atmosphere and heats up the earth like a pizza-oven (making us the pizzas!). However, doctoral student Erik Koepf, from the University of Delaware, has found a way to refine the hydrogen gas without the toxic byproduct which will help in turning down the heat on our pizza-oven atmosphere.

 

To accomplish the earth-friendly process, Erik designed a reactor that uses zinc oxide and concentrated sunlight that essentially kills-off the carbon dioxide, sort of like a natural filter. His reactor uses gravity to disperse the zinc oxide which is housed in 15 ‘hoppers’ located on top of a hollow cylinder (comprised of ceramic materials and insulation). Concentrated sunlight (equaling the energy of 10,000 suns) enters the cylinder from a focal point on top of the reactor that fry’s the zinc on the cylinders ceramic surface. This, in turn, creates zinc vapor, which is then turned into solar-made hydrogen when water is introduced to the vapor cloud. In theory, the byproduct left over from the zinc-oxide reaction could be used again which would make the reactor somewhat self-sustaining. That depends on how many times you could re-use it, so I wouldn’t say indefinitely. The reactor is promising, as future versions could be created on a massive scale that would give us a renewed endeavor for space exploration as well as a viable solution for electric power.

 

Cabe

http://twitter.com/Cabe_e14

  • Sign in to reply
  • DAB
    DAB over 14 years ago

    HI Cabe,

     

    Good post.  I like that this student has realized that CO2 is an element to be used.  Not stored or hated.  Mixing CO2 with other hydro-carbon elements can yield ethanol, methane, complex plastics.

    Hydrogen is a clean fuel, but it has more energy when mixed with other hydrocarbons.

    Hopefully this experiment will encourage others to start thinking of CO2 as a resource.  We have lots of it and each atom could yeild O2, which we kind of need to live.

     

    I am glad people are looking beyond the obvious and are focusing on the true uses of abundant resources.

     

    DAB