Publications
  • Learn
  • More
Publications
Blog Earth has so much garbage in orbit that it’s time to build a ‘Space Fence’
  • Blog
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Publications to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 3 Apr 2012 8:14 PM Date Created
  • Views 1517 views
  • Likes 0 likes
  • Comments 2 comments
  • research
  • test
  • debris
  • industry
  • hmi
  • nasa
  • space
  • tracking
  • cabeatwell
  • prototyping
  • measurement
  • lockheed_martin
  • space_debris
  • sensor
  • innovation
  • communication
Related
Recommended

Earth has so much garbage in orbit that it’s time to build a ‘Space Fence’

Catwell
Catwell
3 Apr 2012

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

The opening the Japanese animated series "Planetes," depicting the fictional first space debris collision on a commuter transport.

 

The earth has so much garbage in orbit that it’s becoming an increasing concern to not only NASA but to the US Air Force, as well. To help with the problem the Air Force has awarded preliminary contracts to both Lockheed Martin and Raytheon Corp. ($107,000,000 US. each) for the AF’s ‘Space Fence’ program which will be used to track small (1 to 10 centimeters in size) orbiting debris that can cause considerable damage to both satellites and space craft. Lockheed’s solution is to develop a ground-based radar system that will be able to locate and identify the tiny space junk. Their design will consist of two to three radar systems that use the S-band range in the electromagnetic spectrum which will enable them to track objects or microsatellites in low-earth orbit at about the size of a basketball. These radar stations will be placed strategically around the globe which will provide ‘Fence’ coverage even in the southern hemisphere.

 

image

Ground based radar tracking system for space debris (via Lockheed Martin)

 

Raytheon has a similar approach to Lockheed which also uses a system of ground-based S-band radars to help in low-orbit earth detection of space garbage. However, Raytheon’s prototype system is already in the testing phase, actively tracking space debris, and was demonstrated to the Air Force back in January of 2012. Both systems so far have been successful in preliminary tracking tests and are more than capable of the task for which they were designed, but there can only be one winner. The victor will be chosen later this year with the winning system fully implemented by 2017. Lets hope a space debris solution is chosen before regular civilian commuter flights head into orbit.

 

Cabe

http://twitter.com/Cabe_e14

 

Other Space Debris Cleanup related news:

New satellite aims to chase down and clean up space debris

NASA to shoot lasers at space debris

SETI to re-start looking for life elsewhere, and track garbage

Space debris threatens the Space Station

Russian POD orbital debris collector

  • Sign in to reply
Parents
  • tarz
    tarz over 14 years ago

    What we need is Sanford & Son.

     

    Compelling article, though. What we really need is an international effort to limit future debris.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Catwell
    Catwell over 14 years ago in reply to tarz

    Eventually, the debris will collect into a ring surrounding the planet, much like Saturn. It may look interesting. (After a few thousand or millions of years, that is)

     

    It is a big deal to any company with an item in space. Satellites are often damaged from space debris. There are collisions that do further damage. There will come a point when collection will be critical.

     

    Cabe

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Catwell
    Catwell over 14 years ago in reply to tarz

    Eventually, the debris will collect into a ring surrounding the planet, much like Saturn. It may look interesting. (After a few thousand or millions of years, that is)

     

    It is a big deal to any company with an item in space. Satellites are often damaged from space debris. There are collisions that do further damage. There will come a point when collection will be critical.

     

    Cabe