Publications
  • Learn
  • More
Publications
Blog Eye tracking system looks deep into your eyes - can tell if you’re lying
  • Blog
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Publications to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 16 Apr 2014 7:04 PM Date Created
  • Views 4735 views
  • Likes 1 like
  • Comments 31 comments
  • safety&security
  • eye
  • law
  • 3d_camera
  • eye_tracking
  • law_enforcement
  • cabeatwell
  • sensor
Related
Recommended

Eye tracking system looks deep into your eyes - can tell if you’re lying

Catwell
Catwell
16 Apr 2014

image

SMI RED-oem Remote Eye Tracking platform render. (via SMI)


Law enforcement and federal agencies have been using polygraph machines to detect lies since Cesare Lombroso introduced his blood pressure device back in 1895. Before that? Torture was used as the best method to detect fibs (still is to some extent). Just ask any witch that was present at the Salem Trials and they could probably tell it didn’t work that well. Some analysts will tell you that the eyes are the gateway in detecting if someone is telling the truth or not. They claim the rate a person blinks is a telltale sign of lying as well as not making eye contact or even looking up and to the left or right may be an indication of false pretenses. Some of the early pioneers of computerized polygraph have banded together to form a company, known as Converus, which is developing a new platform that tracks eye movement to detect deception.


The soon-to-be-released EyeDetect device is outfitted with German-based SMI’s (SensoMotoric Instruments) RED-oem Eye Tracking 3D camera system that tracks gaze, eye movement and pupil dilation down to 1/10 of a millimeter. According to Converus, lying causes minute changes in the eye’s behavior because it induces ‘cognitive load’ (psychology- load related to executive control of working memory), which has an effect on eye movement. Think of it like computer RAM that holds on to pieces of data before being replaced by different programs. EyeDetect captures that ocular data and analyses it to assess the ‘likelihood’ of deception while ‘suspects’ answer a series of true or false questions. The company claims the system has an accuracy rate of 85%, which is pretty high in terms of reliability but most courts in the US still don’t allow polygraph tests submitted as evidence. Converus is set to launch their device in April of this year, with Mexico as its first test subject. Businesses will use it for pre-employment screening as well as using it for random testing on employees to weed-out those individuals that accept bribes or are involved in other nefarious activities (there goes police officers and government officials).


C

See more news at:

http://twitter.com/Cabe_Atwell


image

  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 12 years ago in reply to johnbeetem +2
    Some employers are likely to abuse it, simply because they are human and it is easy to abuse power. They may (say) ask something like "will you disclose your employer's secrets assuming your employer is…
  • mcb1
    mcb1 over 12 years ago +1
    Seem to recall this was called a Voight-Kampff machine on Blade Runner back in 1982. mark
  • sqkybeaver
    sqkybeaver over 12 years ago in reply to sqkybeaver +1
    damn auto spell correct, that last word should have been polygrapher.
Parents
  • sqkybeaver
    sqkybeaver over 12 years ago

    A device with a 85% accuracy, used to keep politicians and law enforcement honest, SERIOUSLY?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • johnbeetem
    johnbeetem over 12 years ago in reply to sqkybeaver

    sheldon bailey wrote:

     

    A device with a 85% accuracy, used to keep politicians and law enforcement honest, SERIOUSLY?

    You can tell if some politicians are lying by seeing if their lips are moving -- with better than 85% accuracy image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • johnbeetem
    johnbeetem over 12 years ago in reply to sqkybeaver

    sheldon bailey wrote:

     

    A device with a 85% accuracy, used to keep politicians and law enforcement honest, SERIOUSLY?

    You can tell if some politicians are lying by seeing if their lips are moving -- with better than 85% accuracy image