Publications
  • Learn
  • More
Publications
Blog Fold Up and Go, the micro-EV
  • Blog
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Publications to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 8 Feb 2012 7:42 PM Date Created
  • Views 946 views
  • Likes 1 like
  • Comments 2 comments
  • research
  • transportation
  • mit
  • industry
  • hmi
  • electric_vehicle
  • robotics
  • ev
  • robot
  • on_campus
  • Design
  • cabeatwell
  • prototyping
  • automotive
  • hybrid
  • electric_car
  • university
  • innovation
Related
Recommended

Fold Up and Go, the micro-EV

Catwell
Catwell
8 Feb 2012

imageimage

Hiriko concept images (via MIT)

 

Double saving with this car! You can save money and save room. Hiriko ("of the city") is the name of the double whammy car that can not only fold itself but runs on electric. The inventor is Jose Manual Barroso who is the president of the European Commission, in Brussels. Barroso is working on the project with the Spanish government and the USA's MIT Media Lab. Their goal is to have the Hiriko on Spanish streets by 2014.

 

Being a folding, do not except much room. The rear wheels simply fold right under the chassis, compressing the rear section forward, folding vertically. This makes the car only two-thirds the of the floor real estate of the Smart ForTwo. In other words, it is small when parked. There is only one door to get in and out this two-seater. The last car that opened up in the front was not much of a success, let us hope for the best with this one.

 

Hiriko’s power comes from a four in-wheel motor. Each wheel is independently driven and is steered by the “robot” electric motor. The oddest design feature stated is the system can tug at the drivers fingers via haptic feedback in the steering wheel. Aside from the haptic traditional shaped steering wheel, a joystick control will also be an option, which is undeniably a throw-back option similar to early model automobiles.

 

Unfortunately, you cannot get your hands on one. Only the 20 prototypes are rolling out to street testing in various European and American cities so far. However, in 2014, expect a price tag for the EV Hiriko to be in the $16,000 range.

 

Cabe

http://twitter.com/Cabe_e14

  • Sign in to reply
  • Catwell
    Catwell over 14 years ago in reply to DAB

    Until we are all in these types of vehicles, I think these will remain in the niche market. Or squished under an H2 Hummer.

     

    Cabe

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 14 years ago

    I like it.

    When you consider the number of cars driving each day with only one person in them and couple that with the fact that the cars then sit idle for eight hours or so each day, this approach makes a lot of sense.

    You reduce the energy needed to move people around.

    You reduce traffic volume.

    You reduce parking space need.

     

    The only other thing I would add is a robot mode where the car could drive itself to the person who needs one that is not available at their location.

    The potential for urban driving needs is very high.  Production would lower the cost and if you set up a credit card swipe for use, you have a self contained method of public transportation.

     

    Neat idea.

    DAB