Publications
  • Learn
  • More
Publications
Blog Garbage sort robot, digging for gold
  • Blog
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Publications to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Eavesdropper
  • Date Created: 7 Apr 2011 10:44 PM Date Created
  • Views 444 views
  • Likes 1 like
  • Comments 1 comment
  • dit
  • eavesdropper:dit
  • robotics
  • robot
  • recycle
  • energy
Related
Recommended

Garbage sort robot, digging for gold

Eavesdropper
Eavesdropper
7 Apr 2011
image
 
A shocking statistic, 40% of all U.S. waste is from construction. Only 20% of that is recycled, and tons of raw material is just packed back into the earth. ZenRobotics looks to change that recycling figure. Their "Recycler ZR M2" can identify useful, recyclable, waste and sort it from the main stream. Using an array of sensors, like visible spectrum camers, NIR, Haptic, transillumination, 3D laser scanners, weight, and metal detectors to accurately sort the waste as it passes down the ZR M2's chambers. The device can also remove unwanted materials from the bit of interest, as in concrete from a support bar or electronics from a steel cabinet.
 
The ZR M2 is already being use in a testing atmosphere, and has learned to identify up to half of the construction waste. This will undoubtedly save in raw material resources and landfill expenses.
 
Lead researcher at ZenRobotics, Tuomas J. Lukka, said he envisions "the robot could one day sort household waste as well."
 
Eavesdropper
 
  • Sign in to reply
  • Former Member
    Former Member over 14 years ago
    I recently saw some pieces on shows like CNN and the journal with Joan Lunden on PBS that were talking about issues and solutions for industrial recycling.  This is an interesting twist that could really become a game changer in the future. Whoever gets in at the beginning of the urban mining will possibly be a part of a new gold rush of sorts.  I hope we start implementing such programs early on to reduce our dependence.
    • Cancel
    • Vote Up 0 Vote Down