Publications
  • Learn
  • More
Publications
Blog Graphene edge states open up new possibilities
  • Blog
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Publications to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Eavesdropper
  • Date Created: 12 May 2011 6:24 PM Date Created
  • Views 553 views
  • Likes 1 like
  • Comments 1 comment
  • dit
  • graphene
  • eavesdropper:dit
  • spintronics
  • on_campus
  • university
  • innovation
Related
Recommended

Graphene edge states open up new possibilities

Eavesdropper
Eavesdropper
12 May 2011
image
 
It was impossible to see the edge-states of a graphene nano-ribbon until now. Before, only theoretical predictions could be made. Michael Crommie, of Berkeley Lab's Materials Sciences Division and UC Berkeley's Physics Division, used a scanning tunneling microscope on specially made graphene nano-ribbons and confirmed all the theoretical predications. The results of his research could lead to faster electronics, energy efficient nano-devices from these graphene nano-ribbons. More remarkable, electron charge and spin can be controlled at the edge-states. (See spintronics)

image
 
Using a special chemical process, graphene nano-tubes can be cut, un-zipped, in such a way that raised edges can be produced, also known as are-chair edges. It is at these scalloped edges that new potentials can be exploited. Crommie explains, "Two-dimensional graphene sheets are remarkable in how freely electrons move through them, including the fact that there's no band gap. Nanoribbons are different: electrons can become trapped in narrow channels along the nanoribbon edges. These edge-states are one-dimensional, but the electrons on one edge can still interact with the edge electrons on the other side, which causes an energy gap to open up...  We might also imagine spintronics applications, where using a side-gate geometry would allow control of the spin polarization of electrons at a nanoribbon's edge."
 
Controlling the edges is key to this discovery. The next step for Crommie and his team is to reproduce the arm-chair edges at a larger scale. As well as continuing the validation. Read more here.
 
Eavesdropper
  • Sign in to reply
  • DAB
    DAB over 14 years ago

    One thing I learned in advanced calculus was that the edge effects can produce some really neat reactions when dealing with materials and electronic signals.  Think what we could do with a controlled energy flow along a single Graphene edge.  The thought of such a cutting device opens a huge amount of potential applications.

     

    Thanks

    DAB