Publications
  • Learn
  • More
Publications
Blog Graphene RF Mixer at 10GHz, 1db loss
  • Blog
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Publications to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Eavesdropper
  • Date Created: 10 Jun 2011 7:30 PM Date Created
  • Views 577 views
  • Likes 1 like
  • Comments 2 comments
  • research
  • intel
  • dit
  • graphene
  • eavesdropper:dit
  • industry
  • ic_mixer
  • rf
  • sensor
  • innovation
Related
Recommended

Graphene RF Mixer at 10GHz, 1db loss

Eavesdropper
Eavesdropper
10 Jun 2011
imageimage
Concept and prototype images
 
Graphene continues on its road to adoption with Intel's demonstration of a Graphene based analog broadband Radio Frequency Mixer. The mixer, a signal summing device, produces an output signal from the mixing of the input frequencies. In other words, adding up the several input signals to produce a single clean and distortion free version of the input.
 
Intel's graphene mixer operates up to 10GHz at temperatures between 25°C and 125°C with very little loss, 1 decibel between temp range. A 27 decibel conversion loss was experience at 4GHz. The circuit did not need any external passive components, making this particular mixer cheaper and more attractive for use in future wireless devices. With Intel demonstrating their 155GHz transistor, higher frequencies could open up for this wireless mixer to use.
 
Graphene's energy gap ratio is still not deep enough to create true on/off capabilities, so it is some time away from replacing our CPUs. However, for analog situations like the RF mixer, graphene is an ideal candidate for use.
 
Another fun graphene discovery; Auto-cooling components.
 
Eavesdropper
 
Pictures from Intel
  • Sign in to reply
  • Eavesdropper
    Eavesdropper over 14 years ago in reply to DAB

    If research could figure a way to widen the energy gap, we would have a revolution of technological possibilities.

     

    E

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 14 years ago

    The more they look at Graphene, the more potential they will find.  The open structure promotes high frequency operation, plus it opens the potential for moving small particles using the resulting magnetic fields inside the structure.  The mind boggles at the posibilities.

     

    DAB