Publications
  • Learn
  • More
Publications
Blog IBM and Micron Technology confirm work on revolutionary 3D memory chip
  • Blog
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Publications to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Joshua_Evans
  • Date Created: 8 Dec 2011 5:36 PM Date Created
  • Views 834 views
  • Likes 1 like
  • Comments 2 comments
  • news_a
Related
Recommended

IBM and Micron Technology confirm work on revolutionary 3D memory chip

Joshua_Evans
Joshua_Evans
8 Dec 2011

IBM and Micron Technology have confirmed that they are beginning to produce a new memory chip based on technology which could boost memory speeds 15-fold. It has been announced that the new technology will be used to make a Hybrid Memory Cube chip.
The chip will be commercially manufactured by Micron, the largest manufacturer of memory chips in the US. IBM, meanwhile, has announced that it plans to manufacture and supply the "controller" silicon, which will ultimately be used in the memory and the 3D-chip technology.
The long-term ambition of the project is to realize the full performance potential of DRAM (dynamic random access memory). By doing so, it is hoped that the technology will resolve a growing problem referred to as the "memory wall" –a data channel bottleneck created by multi-core processors seeking access to memory.
Initially, however, the technology will be used in areas such as networking and high-performance computing. But over time, Micron and IBM feel that the technology will eventually make its way to consumer products.
IBM's technology is based on through-silicon vias (TSV), which use vertical conduits to electrically connect a stack of individual chips. It has been confirmed that the technology will be combined with Micron's state-of-the-art DRAM processes.
In a statement, the world's second most valuable technology firm explained: "IBM's advanced TSV chip-making process enables Micron's Hybrid Memory Cube to achieve speeds 15 times faster than today's technology."
The firm added that while current state-of-the-art devices deliver 12.8GBps (gigabytes per second), Hybrid Memory Cube chips are able to offer speeds of 128GBps.. Furthermore, IBM said that the Cube requires 70 percent less energy to transfer data and also offers a more compact design. It is, in fact, around ten percent of the footprint of conventional memory.
Micron is the founding member of the Hybrid Memory Cube Consortium, which includes Altera,  Intel, Open Silicon, Samsung and Xilinx.
IBM said that it will manufacture its Hybrid Memory Cube components at its semiconductor plant in New York. To this end, the firm revealed that it will use its 32-nanometer high-K metal gate process technology.
"Our ability to use TSVs in commercial ... production and integrating other chip technology, such as high-speed communications, is a key advancement in the move to 3D semiconductor manufacturing," explained IBM Fellow Subu Iyer.
Although IBM has refused to specify a date, it is speculated that the chips will start shipping in the second half of 2012.

IBM and Micron Technology have confirmed that they are beginning to produce a new memory chip based on technology which could boost memory speeds 15-fold. It has been announced that the new technology will be used to make a Hybrid Memory Cube chip.

 

The chip will be commercially manufactured by Micron, the largest manufacturer of memory chips in the US. IBM, meanwhile, has announced that it plans to manufacture and supply the "controller" silicon, which will ultimately be used in the memory and the 3D-chip technology.

 

The long-term ambition of the project is to realize the full performance potential of DRAM (dynamic random access memory). By doing so, it is hoped that the technology will resolve a growing problem referred to as the "memory wall" – a data channel bottleneck created by multi-core processors seeking access to memory.

 

Initially, however, the technology will be used in areas such as networking and high-performance computing. But over time, Micron and IBM feel that the technology will eventually make its way to consumer products.

 

IBM's technology is based on through-silicon vias (TSV), which use vertical conduits to electrically connect a stack of individual chips. It has been confirmed that the technology will be combined with Micron's state-of-the-art DRAM processes.

 

In a statement, the world's second most valuable technology firm explained: "IBM's advanced TSV chip-making process enables Micron's Hybrid Memory Cube to achieve speeds 15 times faster than today's technology."

 

The firm added that while current state-of-the-art devices deliver 12.8GBps (gigabytes per second), Hybrid Memory Cube chips are able to offer speeds of 128GBps.. Furthermore, IBM said that the Cube requires 70 percent less energy to transfer data and also offers a more compact design. It is, in fact, around ten percent of the footprint of conventional memory.

 

Micron is the founding member of the Hybrid Memory Cube Consortium, which includes Altera,  Intel, Open Silicon, Samsung and Xilinx.

 

IBM said that it will manufacture its Hybrid Memory Cube components at its semiconductor plant in New York. To this end, the firm revealed that it will use its 32-nanometer high-K metal gate process technology.

 

"Our ability to use TSVs in commercial ... production and integrating other chip technology, such as high-speed communications, is a key advancement in the move to 3D semiconductor manufacturing," explained IBM Fellow Subu Iyer.

 

Although IBM has refused to specify a date, it is speculated that the chips will start shipping in the second half of 2012.

  • Sign in to reply
Parents
  • DAB
    DAB over 14 years ago

    This technology reminds me of the crystal memory devices used on the old SciFi TV show Babylon 5 to store huge volumes of data in small spaces.

    I also remember when magnetic bubbles were going to do this for us, and then there was the optical disks, solid state memory, optical computers, and others.  So when they reach my desk, then I will celebrate a true accomplishment.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 14 years ago

    This technology reminds me of the crystal memory devices used on the old SciFi TV show Babylon 5 to store huge volumes of data in small spaces.

    I also remember when magnetic bubbles were going to do this for us, and then there was the optical disks, solid state memory, optical computers, and others.  So when they reach my desk, then I will celebrate a true accomplishment.

     

    DAB