Publications
  • Learn
  • More
Publications
Blog Inkjet printed solar panels
  • Blog
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Publications to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Eavesdropper
  • Date Created: 7 Jul 2011 5:49 PM Date Created
  • Views 504 views
  • Likes 1 like
  • Comments 2 comments
  • research
  • dit
  • eavesdropper:dit
  • on_campus
  • inkjet
  • printing
  • university
  • solar
  • innovation
Related
Recommended

Inkjet printed solar panels

Eavesdropper
Eavesdropper
7 Jul 2011
image
Chalcopyrite deposit via Oregon State University
 
Sometimes many people around the world have the same idea simultaneous. Then a resounding, "that was my idea," is heard as someone actually attempts to act on the thought.
 
Has this ever occurred to you? Printing a solar panel.
 
Oregon State University can make solar panels with inkjet printing techniques. Not only that, but the new panels reduce material waste by 90%. The low cost, thin film solar electronics have a power conversion rate at 5% currently, and 12% may be achievable soon. 12% puts it on par with the average thin film solar panels used today, and on the lower end of traditional silicon. "This is very promising and could be an important new technology to add to the solar energy field," said professor of Chemical, Biological, and Environmental Engineering Chih-hung Chang.
 
"Until now no one had been able to create working CIGS solar devices with inkjet technology," Chang continued. The new "CIGS" based solar panel consists of copper, indium, gallium, and selenium, also known as chalcopyrite. The solar efficiency at two microns is equivalent to 50-micron silicon. The research team created an ink that could print the chalcopyrite layers on a substrate with the inkjet technique. “Some of the materials we want to work with for the most advanced solar cells, such as indium, are relatively expensive,” Chang said. “If that’s what you’re using you can’t really afford to waste it, and the inkjet approach almost eliminates the waste.”
 
The work was funded by the "Daegu Gyeongbuk Institute of Science and Technology, the U.S. Department of Energy and OSU’s University Venture Development Fund, which helps donors receive tax benefits while sponsoring projects that will bring new technology, jobs and economic growth to Oregon."
 
Looks like Dyesol and Tata Steel better ramp up their printed solar efforts.
 
Eavesdropper
  • Sign in to reply
  • Eavesdropper
    Eavesdropper over 14 years ago in reply to DAB

    Acording to the Solarbuzz United States Deal Tracker database, nonresidential photovoltaic project pipeline exceeds 17 giga-watts, and will be 20.3 giga-watts by 2015. What they are showing is a jump in the adoption of solar projects by states in direct relation to the falling of solar panel prices. Older technology is getting cheaper, newer thin-film solar is also cheaper than ever. It is going to happen, and soon.

     

    E

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 14 years ago

    I agree, the easier the solar collectors are to make, then you can ramp up the numbers to overcome their lack of efficiency by putting them everywhere.  The cost is the key.  If they are cheap and easy to install, then you have a viable solar collection system.

    If they are just printed on, then you can wear them in the sun and power your mobile devices.

    We have the technology, it is just an issue of production, integration and use on a wide scale.

     

    DAB