Publications
  • Learn
  • More
Publications
Blog Intel introduces inexpensive ULV processors for ultra-thin notebooks
  • Blog
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Publications to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 23 May 2012 5:45 PM Date Created
  • Views 750 views
  • Likes 1 like
  • Comments 2 comments
  • fabrication
  • research
  • intel
  • industry
  • Design
  • cabeatwell
  • prototyping
  • gpu
  • cpu
  • fab
  • apu
  • innovation
Related
Recommended

Intel introduces inexpensive ULV processors for ultra-thin notebooks

Catwell
Catwell
23 May 2012

image

The ULV chips in progress (via Intel)

 

Intel  announced the release of a series of mobile ULV (ultra-low voltage) processors for ultra-book manufacturers such as MSI, Acer, ASUS and a host of others. The chips include the entry-level Celeron family including the ULV 807 (1.05GHZ), 877 (1.04GHz) and the U3400 (1.03GHz) made using Intel’s new 32 nanometer wafer manufacturing process and cost $70 US, $86 US and $134 US respectively. The company states that these new chips are not only 32% smaller over the previous generation of Celeron mobile processors but also feature a 32% increase in overall performance.

 

The company is also releasing a next generation of Ivy Bridge dual-core mobile processors that include the Core i3 330M (2.13GHz), Core i5 520UM (1.06GHz) and Core i7 620M (2.66GHz) priced at $225 US, $241 US and $332 US respectively. These processors feature Hyper-Threading and Turbo-Boost technology, which overclocks the processor for increased speed based on workloads. In all, these new processors chew-up less power than the previous gen by more than 15% resulting in longer battery life for the up-coming netbooks. Intel say’s that more than 40 different designs from the various manufacturers are expected with their price-point based on 1000 units for the OEM’s only. It’s Intel’s hope that the reduced prices of the new processors will result in cheaper notebooks with prices starting at $699 US and dropping to $599 US by the end of this year or the beginning of next year (2013) and we can expect to see the first of these notebook designs starting in June.

 

Cabe

http://twitter.com/Cabe_e14

  • Sign in to reply
Parents
  • DAB
    DAB over 14 years ago

    It's too bad that Intel has moved away from the DIY customers. 

    Given the volume of commercial sales, I can't blame them, but it keeps these really powerful chips out of the maker market.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Catwell
    Catwell over 14 years ago in reply to DAB

    Mobility and miniaturization has made it difficult for the average person to handle properly. Where a 2"x2" square is easy to see and hold, while the single-digit-milimeter chips are not. Also, the smaller chips are far more susceptible to ESD.

     

    I do hope we all can build our own cell phones someday. (And not like this one.)

     

    Cabe

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Catwell
    Catwell over 14 years ago in reply to DAB

    Mobility and miniaturization has made it difficult for the average person to handle properly. Where a 2"x2" square is easy to see and hold, while the single-digit-milimeter chips are not. Also, the smaller chips are far more susceptible to ESD.

     

    I do hope we all can build our own cell phones someday. (And not like this one.)

     

    Cabe