Publications
  • Learn
  • More
Publications
Blog Intel processor running below 1V
  • Blog
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Publications to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Eavesdropper
  • Date Created: 4 Oct 2011 6:58 PM Date Created
  • Views 551 views
  • Likes 1 like
  • Comments 1 comment
  • alternative_energy
  • eavesdropper:dit
  • hmi
  • microprocessor
  • energy
  • sensor
  • innovation
  • communication
Related
Recommended

Intel processor running below 1V

Eavesdropper
Eavesdropper
4 Oct 2011
image
Claremont prototype (via Intel)
 
Intel has recently developed technology that seems to be years ahead of time. This time it is a solar-powered  microprocessor, code-named Claremont, with a low-energy mode of less than 10 milli-watts, that allows for applications to be constantly running.
 
According to Intel, the purpose of the Claremont processor is to achieve unparalleled energy efficiency. Most embedded chips operate at nominal voltage of about 1V today. Claremont, dubbed the "Near threshold voltage" processor, can function at around 400-500 millivolts. “Threshold” voltage is the point at which transistors turn on and begin to conduct current. It is challenging to run electronics reliably at such voltage levels.
 
As of yet Intel has not decided whether or not to produce the Claremont. However, it is exciting because it could open the door to a whole new generation of computing technology. With technology like this you have been claims of boasting 10 times the computing power and cutting power consumption by 1/10. With these types of power demands, future mobile devices could be run on solar power, wireless energy harvesting, sound, or even off the heat in one's own pocket.
 
Eavesdropper
  • Sign in to reply
  • fustini
    fustini over 14 years ago

    Can't wait to have a tablet that is powered off the energy of me touching it image

     

    It's rather amazing though if it uses 500mV logic, then the margin for high and low levels must be very sensitive.  I guess this is only viable for internal core functioning and not interfacing circuitry?

    • Cancel
    • Vote Up 0 Vote Down