Publications
  • Learn
  • More
Publications
Blog lens-less micro camera
  • Blog
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Publications to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Eavesdropper
  • Date Created: 7 Jul 2011 5:47 PM Date Created
  • Views 653 views
  • Likes 1 like
  • Comments 2 comments
  • research
  • dit
  • eavesdropper:dit
  • on_campus
  • camera
  • university
  • medical
  • sensor
  • innovation
Related
Recommended

lens-less micro camera

Eavesdropper
Eavesdropper
7 Jul 2011
What could be done with a lens-free camera that is half a millimeter square and 100th of a millimeter thick with a 20 pixel diagonal resolution?
 
From the Cornell University lab of Alyosha Molnar comes the "Planar Fourier Capture Array" (PFCA) camera. Using the principles of Fourier transforms, information can be captured in many ways. Each pixel in the PFCA reports the Fourier transform of a unique blend of incident angles. In other words, a direct image is not taken. Instead a little bit of math can transform the Fourier components into the picture.
 
The PFCA was developed as a side project to image brain activity by group leader and postdoctoral associate Patrick Gill. The camera is doped silicon disc with no moving parts or off-chip manufacturing steps.  As a result it is small, light, and only costs a few cents to make. And currently the team seeks to increase the resolution and efficiency.
 
How I would put this new camera to work. Using sixteen of these cameras together would give an adequate resolution and favorable size for use in the Mermaid medical robot. Two millimeters is easier to take than comparably monstrous 10 millimeter diameter the robot is now.
 
Eavesdropper
  • Sign in to reply
Parents
  • DAB
    DAB over 14 years ago

    I can envision a number of interesting applications for this type of sensor.  Notice I said sensor, not camera.  Having a small sensor with the full range of silicon sensitivity could be very useful to detect small scale biological and nonbiological instances in remote locations.  Think about finding a virus that survives your decontamination bath, but could only be found through passing a fluid over these types of sensors.

     

    I'll bet there are a lot of wheels spinning in peoples heads over the possibilities of these things.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 14 years ago

    I can envision a number of interesting applications for this type of sensor.  Notice I said sensor, not camera.  Having a small sensor with the full range of silicon sensitivity could be very useful to detect small scale biological and nonbiological instances in remote locations.  Think about finding a virus that survives your decontamination bath, but could only be found through passing a fluid over these types of sensors.

     

    I'll bet there are a lot of wheels spinning in peoples heads over the possibilities of these things.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • Eavesdropper
    Eavesdropper over 14 years ago in reply to DAB

    I think it is a medical science holy grail to have cameras and "bots" in the blood stream able to see and interact with a single virus. Until single molecule electronics pick up in development, we probably will not see anything close to what you want to see.

     

    According to this, I could be wrong.

     

    E