Publications
  • Learn
  • More
Publications
Blog Light-harvesting at 100%
  • Blog
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Publications to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Eavesdropper
  • Date Created: 7 Sep 2011 7:22 PM Date Created
  • Views 536 views
  • Likes 1 like
  • Comments 2 comments
  • research
  • alternative_energy
  • eavesdropper:dit
  • on_campus
  • university
  • energy
  • solar
  • innovation
Related
Recommended

Light-harvesting at 100%

Eavesdropper
Eavesdropper
7 Sep 2011
image
(Diagram via Tokyo Metropolitan University and Shinsuke Takagi)
 
 
At the Tokyo Metropolitan University and the Japan Science and Technology Agency, researcher Shinsuke Takagi led a team in realizing an artificial light-harvesting system (LHS) that achieves up to 100% efficiency. The LHS, or "artificial leaf," works off the same principle of real leaves, by arranging molecules to collect the light and carry the energy to the system's "reaction center."
 
Two types of porphyrin dye molecules were used on a clay surface. It was a challenge to arrange the molecules to work properly. Takagi explained, "A molecular arrangement with an appropriate intermolecular distance is important to achieve nearly 100% energy transfer efficiency. If the intermolecular distance is too near, other reactions such as electron transfer and/or photochemical reactions would occur. If the intermolecular distance is too far, deactivation of excited dye surpasses the energy transfer reaction.” 
 
In what is called the "Size-Matching Rule," the team was able to arrange the molecules by matching distances between charged porphyrin molecules and between negatively charged anionic sites on the clay. This stops much of the "aggregation" and "segregation" of the porphyrin molecules, which create chaotic, non-uniform, patterns on the surface. To make get to the efficiencies needed, a precise uniform pattern is needed, like in real leaf structures.
 
Takagi spoke about his plans for future use of the technology, "At the present, our system includes only two dyes. As the next step, the combination of several dyes to adsorb all sunlight is necessary. One of the characteristic points of our system is that it is easy to use several dyes at once. Thus, our system is a promising candidate for a real light-harvesting system that can use all sunlight. We believe that even photochemical reaction parts can be combined on the same clay surface. If this system is realized and is combined with a photochemical reaction center, this system can be called an ‘inorganic leaf.’”
 
Eavesdropper
  • Sign in to reply
Parents
  • DAB
    DAB over 14 years ago

    An interesting approach, but I am not sure how well it can be produced for mass use.  Good step in the right direction though.  It will be interesting to see how their technology progresses.

     

    Thanks

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Catwell
    Catwell over 14 years ago in reply to DAB

    I see now that near 100% solar is amost here. I can not wait.

     

    Cabe

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Catwell
    Catwell over 14 years ago in reply to DAB

    I see now that near 100% solar is amost here. I can not wait.

     

    Cabe