Publications
  • Learn
  • More
Publications
Blog Los Angeles replaces aging streetlights with more efficient LEDs, about time...
  • Blog
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Publications to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 27 Sep 2013 5:30 AM Date Created
  • Views 916 views
  • Likes 0 likes
  • Comments 2 comments
  • research
  • alternative_energy
  • transportation
  • la
  • industry
  • los_angeles
  • lighting
  • usa
  • led
  • cabeatwell
  • energy
  • innovation
  • street_lights
Related
Recommended

Los Angeles replaces aging streetlights with more efficient LEDs, about time...

Catwell
Catwell
27 Sep 2013

image

Clinton Climate Initiative LED streetlight... Los Angeles - now the "City of LED Lights" (via LA Bureau of Street Lighting)

 

 

Street lighting has been around since the ancient Romans and Greeks used them for safety purposes (tripping over obstacles, etc.) and to keep thieves at bay. Those were of course oil lamps and were in use all over the globe until 1875 when Russian inventor Pavel Yablochkov introduced his ‘Yablochkov Candle’ to the world. The first use of his electric lamp was in Paris where 80 of them were deployed to light the Grand Magasins du Louvre department store, which is where the city subsequently earned its nickname ‘The City of Lights’. Since that time, electric incandescent street lights in one form or another have been used to illuminate highways and on/off ramps for over 100 years, however this is about to change.

 

LEDs have proven to be much more efficient  than traditional incandescent lamps when it comes to power use, so it was only natural that the Los Angeles Bureau of Street Lighting used them to replace the city’s aging streetlights. The city’s Light Emitting Diode Street Lighting Retrofit (part of the Clinton Climate Initiative), has replaced over 140,000 of their streetlights with more efficient LED units over the past four years. As a result of switching over to LEDs, the city’s energy use for lighting has been reduced by over 62% and carbon emissions were reduced by over 47,000 metric tons per year. The city’s light pollution has also been reduced due to using white LEDs, which is also getting high-praise from the LAPD as well as the Dark Skies Association (the premier authority on light pollution). Los Angeles isn’t the only city to make the transformation over to LED street lighting, as Las Vegas replaced 42,000 lights back in May of this year and Austin is looking to replace 35,000 of their lights. San Antonio is set to install 20,000 LED lights as well, as the trend to go green is taking the US by storm.

 

The adoption of LED lighting has been steadily increasing over the years from 3 million units in the beginning of 2012 and is expected to grow to over 17 million by the year 2020. This is to be expected as the demand for energy has been increasing over the last few decades as more countries have been expanding their infrastructure. The benefits of using LED lighting are obvious, LA alone has reduced its electric bill by 7 million dollars with an additional savings of 2.5 million through reduced maintenance expenditures. The city isn’t finished with replacing the defunct high-pressure sodium fixtures, as they plan to switch out an additional 70,000 units with the second phase of their initiative, which is expected to be completed by 2014. The total budget to replace those fixtures tops out at $56.9 million, which may sound like a lot of money but considering the savings that will accumulate over a period of a few years will save the city money in the long run.

 

C

See more news at:

http://twitter.com/Cabe_Atwell

  • Sign in to reply
Parents
  • DAB
    DAB over 13 years ago

    Hopefully they have already checked to see if the new street lights reduce light pollution for astronomers.

     

    The big issue with the older lamps was all of the wasted energy emitted during use that just filled the air with stray light.

    I have not seen any studies on the light pollution aspects of LED's, but there could still be an issue if they are emitting in visible light or infrared spectrums.

     

    Still, given the cost of power, you have to wonder what they are waiting for.  The cost to replace is probably about a year or so and the replacement cycle probably runs into years of extended life before replacement needs.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 13 years ago

    Hopefully they have already checked to see if the new street lights reduce light pollution for astronomers.

     

    The big issue with the older lamps was all of the wasted energy emitted during use that just filled the air with stray light.

    I have not seen any studies on the light pollution aspects of LED's, but there could still be an issue if they are emitting in visible light or infrared spectrums.

     

    Still, given the cost of power, you have to wonder what they are waiting for.  The cost to replace is probably about a year or so and the replacement cycle probably runs into years of extended life before replacement needs.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to DAB

    DAB wrote:

    The cost to replace is probably about a year or so

    The original article says the cost-recovery period is 7 years (maybe not including interest payments).

     

    This proposal has generated savings in energy and maintenance costs that will pay for the estimated loan amount in seven years with no adverse impact to the General Fund.

    $57M cost resulting in estimated $7M/yr electricity savings and $2.5M maintenance savings.

    Lifetime of LEDs is estimated at 10-15 yrs.

    http://www.forbes.com/sites/justingerdes/2013/01/25/los-angeles-saves-millions-with-led-street-light-deployment/