Publications
  • Learn
  • More
Publications
Blog Low-cost Carbon Nanotubes, drawn with a pencil
  • Blog
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Publications to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 15 Oct 2012 6:25 PM Date Created
  • Views 622 views
  • Likes 1 like
  • Comments 1 comment
  • research
  • mit
  • industry
  • hmi
  • on_campus
  • cabeatwell
  • prototyping
  • carbon_nanotube
  • university
  • innovation
  • communication
Related
Recommended

Low-cost Carbon Nanotubes, drawn with a pencil

Catwell
Catwell
15 Oct 2012

image

Drawing with carbon nanotubes? (via MIT & Jan Schnorr)

 

Development surround Carbon Nanotubes continue to surprise and amaze. The electrically conductive material makes for an acute sensor. In particular, it can detect the presence of gases as a drastic change of their conductivity occurs when certain gasses stick to the nanotubes. Coating them with polymers of different substances can change which gases they interact with. Copper coatings, for example, are used to detect ethylene gas that is released during the ripening of fruit and could be used for better food management.

 

 

A problem with these sensors is that they imply the use of nanotube solvents, like dichlorobenzene, that are toxic, harmful and not entirely reliable, to deposit the nanotubes onto gas-detecting circuits. MIT postdoctoral Katherine Mirica and her team have developed a new method that facilitates their application and does not require these harmful chemicals.

 

 

Mirica was able to compress commercially available single-walled carbon nanotube (SWCNT) powders to resemble a more common form of carbon, pencil lead. The compression is just enough to hold the nanotubes to a solid form but layers of them can be deposited on paper much like regular pencil lead. Handling and application of SWCNT in this compressed form is incredibly safe and stable. Sensors made using this nanotube lead work better on smoother papers and the team found that the marks do not have to be uniform for functionality. The team drew an SWCNT layer to connect gold electrodes and created a sensor that detects ammonia.

 

 

These hand-drawn sensors can detect gases in concentrations of 0.5 parts per million. This research has scientists hopeful towards mass producing sensors, cheaply and in a safe manner, that detect all sorts of volatile gases like sulfur compounds, natural gas etc. The team was lead by Timothy Swager, a John D. MacArthur Professor of Chemistry and the research was funded by the Army Research Office through MIT’s Institute for Soldier Nanotechnologies and a National Institutes of Health fellowship.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

 

Cabe

http://twitter.com/Cabe_e14

  • Sign in to reply
Parents
  • DAB
    DAB over 13 years ago

    What I like most about the carbon nanotube potential is that it looks like it could easily lead to being constructed in a simple 3D printer.

     

    Consider this approach.  You can setup a design for different sensor types.  After you specify the sensitivity and size issues, you could have a 3D printer assemble the sensor using simple materials like graphite and some other easy to use materials and print out your sensor.

    You would have a simple standard interface by which you could then attach your sensor to your data acquisition device and from their, it is just an issue of collecting your data and analysing the results.

     

    Think about the science we could do in remote areas with this level of versatile technology, be it the ocean, mountains, deserts, the moon, Mars, etc.

    You could even have a robot explorer create new sensors based upon what information it uncovers on the spot.  No need to wait 5-10 years before we build and send a new sensor set.

    This approach would also greatly improve terrestrial exploration.  We have only looked at about 10% of the earths surface area and even less of the earths interior. 

    Carbon nanotechnology could help us deal better with all of our undiscovered resources litterally under our feet and under the water.

     

    Just my opinion,

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 13 years ago

    What I like most about the carbon nanotube potential is that it looks like it could easily lead to being constructed in a simple 3D printer.

     

    Consider this approach.  You can setup a design for different sensor types.  After you specify the sensitivity and size issues, you could have a 3D printer assemble the sensor using simple materials like graphite and some other easy to use materials and print out your sensor.

    You would have a simple standard interface by which you could then attach your sensor to your data acquisition device and from their, it is just an issue of collecting your data and analysing the results.

     

    Think about the science we could do in remote areas with this level of versatile technology, be it the ocean, mountains, deserts, the moon, Mars, etc.

    You could even have a robot explorer create new sensors based upon what information it uncovers on the spot.  No need to wait 5-10 years before we build and send a new sensor set.

    This approach would also greatly improve terrestrial exploration.  We have only looked at about 10% of the earths surface area and even less of the earths interior. 

    Carbon nanotechnology could help us deal better with all of our undiscovered resources litterally under our feet and under the water.

     

    Just my opinion,

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
No Data