Publications
  • Learn
  • More
Publications
Blog Medical results in minutes, Collaboration aims to develop lab-on-a-chip through digital microfluidics
  • Blog
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Publications to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 22 Jun 2012 5:13 PM Date Created
  • Views 844 views
  • Likes 1 like
  • Comments 2 comments
  • research
  • test
  • hmi
  • on_campus
  • Design
  • cabeatwell
  • prototyping
  • measurement
  • university
  • medical
  • technology_for_the_disabled
  • innovation
  • communication
Related
Recommended

Medical results in minutes, Collaboration aims to develop lab-on-a-chip through digital microfluidics

Catwell
Catwell
22 Jun 2012

image

Bed Hadwen with the lab-on-a-chip device (via University of Southampton)

 

The hospital waiting room could turn into the place one waits for all their results. A team of researchers from Sharp Labs Europe in collaboration with the University of Southampton has recently announced their combined effort in developing a pocket sized device that analyzes blood in a matter of minutes rather than days. The team, led by Sharp’s Ben Hadwen, developed the lab-on-a-chip using what’s known as ‘digital microfluidics’ which processes tiny (nano-liter) discrete droplets of fluid (in this case blood) that can be mixed, reacted and analyzed using either electrowetting (manipulation from an applied electrical field), dielectrophoresis (manipulation from a non-uniform electrical field) or immiscible-fluid flows.

 

The team’s device works by placing a droplet of blood on the devices microfluidic square (4 to 5cm) where it is then broken down into smaller sized sub-droplets by the LCD-based micro-electronics located directly underneath the square. The droplets are then subjected to bio-chemical diagnostic testing which can then be analyzed in a matter of minutes. In fact, multiple testing can be done with only one drop of blood because the device is able to split and store the droplets for additional testing. Digital microfluidics isn’t actually new as Cytonix designed microfluidic bio-chips back in 1987 that were EWOD-based (Electrowetting on Dielectric) but the technology was lab-based and certainly not portable.

 

Of course, the team states that their device could also be used to test other liquids such as urine that could detect infections, virus’s or drug use. While Sharp Labs states that the company could easily mass produce, the device is still in its infant stage of development and still needs testing and refinement which could take another 5 to 10 years before it hits the market.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image


Cabe

http://twitter.com/Cabe_e14

  • Sign in to reply
Parents
  • DAB
    DAB over 14 years ago

    I like where this research is going, but we need to see results sooner than ten years.

     

    Let's face it, we could reduce health care costs by at least half if we just put people on reasonable diets.  We are eating ourselves to death for no apparent reason.

     

    Just my opinion,

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 14 years ago

    I like where this research is going, but we need to see results sooner than ten years.

     

    Let's face it, we could reduce health care costs by at least half if we just put people on reasonable diets.  We are eating ourselves to death for no apparent reason.

     

    Just my opinion,

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • Catwell
    Catwell over 14 years ago in reply to DAB

    Food is just too taste. Easier to make healthy alternatives would be the greatest benefit to health in decades.

     

    I agree, quicker development is needed. But there is only so much a handful of people can do in a given time period.

    Perhaps if more people volunteered to help projects they believe in.

     

    Cabe