Publications
  • Learn
  • More
Publications
Blog Microsoft’s Wearable Multitouch Projector puts a touchscreen on any surface
  • Blog
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Publications to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 12 Mar 2012 7:37 PM Date Created
  • Views 604 views
  • Likes 1 like
  • Comments 2 comments
  • research
  • test
  • microsoft
  • industry
  • hmi
  • embedded
  • cabeatwell
  • prototyping
  • touchscreen
  • sensor
  • innovation
Related
Recommended

Microsoft’s Wearable Multitouch Projector puts a touchscreen on any surface

Catwell
Catwell
12 Mar 2012
You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

If you’re looking to use a projected touch screen on any surface while looking like the "Predator" alien from the movies, then Microsoft’s got you, or rather any surface, covered with their Wearable Multitouch Projector. The projector, designed by Chris Harrison, Hrvoje Benko and Andy Wilson is outfitted with a PrimeSense RGB/depth camera (it’s actually an Asus XTION Pro) that can image objects with a 320X240 resolution as close as 20cm at 30fps. Along with the depth camera is an SHOWWX Laser Pico Projector that can project a focus free image (with a range of 6in to 100in) at a resolution of 848X480 at a 16:9 aspect ratio.

 

image

Mounted camera and projector. (via Mircosoft)

 

The R&D guy’s at Microsoft had to calibrate the camera for finger detection by using an algorithm that ‘looks for vertical slices of cylinder-like objects’ which allows the fingers to be separate objects rather than one big one. This enables the user to use any or multiple digits to interact with the screen. For the actual ‘click detection’ the team used a depth map that can detect the distance of an object on a very small scale (a centimeter or less). This enables the system to judge distance and whether the object (or finger) has made contact with the image projected. The combined platform of both camera and projector is placed on the users shoulder because the location provides an unobstructed field-of-view for both projection and interaction.

 

Sure, the Wearable Multitouch Projector is rather large and sure you will look kind of funny wearing it, but it sure is cool being able to make a touchscreen out of everything even curved surfaces. According to the team, future versions could be as small as a matchbox, and it could be worn as a pendant with the continuing miniaturization of technology.

 

Cabe

http://twitter.com/Cabe_e14

  • Sign in to reply
Parents
  • DAB
    DAB over 14 years ago

    Hi Cabe,

     

    This is an interesting approach, but it would be more practcable to use a set of projection led's on a pair of glasses and run the IR hand movement detection so you could use the system without anyone else seeing what you are doing.

    There current approach would be OK for simple searches or media interaction, but would not be suitable for private information.

     

    Just a thought,

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 14 years ago

    Hi Cabe,

     

    This is an interesting approach, but it would be more practcable to use a set of projection led's on a pair of glasses and run the IR hand movement detection so you could use the system without anyone else seeing what you are doing.

    There current approach would be OK for simple searches or media interaction, but would not be suitable for private information.

     

    Just a thought,

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • Catwell
    Catwell over 14 years ago in reply to DAB

    I too would prefer an augmented reality solution. But combining the tracking ability of a Kinect into a pair of glasses at the moment would not look aesthetically pleasing. Nevertheless, it is on the way.

     

    I can't wait.

     

    Cabe