Publications
  • Learn
  • More
Publications
Blog Nanoshells, the solar whispering-gallery
  • Blog
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Publications to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 14 Feb 2012 10:47 PM Date Created
  • Views 556 views
  • Likes 1 like
  • Comments 1 comment
  • research
  • alternative_energy
  • industry
  • on_campus
  • cabeatwell
  • prototyping
  • university
  • energy
  • solar
  • innovation
Related
Recommended

Nanoshells, the solar whispering-gallery

Catwell
Catwell
14 Feb 2012

imageimage

(Left) Cross section of the Nanoshell surface. (Right) How light, in red, propogates through the shells. (via Stanford University)

 

A paper published by a team of engineers at Stanford reveals a new way to capture energy from the sun employing nanotechnology. They made this possible by creating thin solar panels out of hollowed out nanoshells. The nanoshells themselves are made out of photovoltaic nanocrystalline-silicon that are  hollowed out at the center. The nanoshells capture light and due to their concave geometry. The surface of the material acts like a wave guide, forcing the light to circulate inside the shells. The team likened the idea to how sound propagates through a whispering-gallary. As a result, the light is better absorbed by the material due to the increase in time duration of light within the material. With a three layer structure, up to 75% of critical spectrums of light are absorbed.

 

 

Post-doctoral researcher on the project, Yan Yao, explained the benefit, "A micron-thick flat film of solid nanocrystalline-silicon can take a few hours to deposit, while nanoshells achieving similar light absorption take just minutes.... This is a new approach to broadband light absorption. The use of whispering-gallery resonant modes inside nanoshells is very exciting. It not only can lead to better solar cells, but it can be applied in other areas where efficient light absorption is important, such as solar fuels and photodetectors.”

 

 

Additionally, the construction of the nanoshells allows for quick production and many new possible applications.  The material is highly efficient even under heat. The thin construction allows for flexibility which is currently not possible with solar panels. This technology brings a lot of potential for future applications in high-efficiency sun collection industry. So many players in the solar game, if they would only work together.

 

Cabe

http://twitter.com/Cabe_e14

  • Sign in to reply
  • DAB
    DAB over 14 years ago

    Hi Cabe,

     

    Neat discovery.  As I understand it, the design is similar to how a rain drop will focus light to the center and then the energy is equally distributed along the inner surface.  That is what probably makes the PV crystal work.  Plus you get maximum heat dissipation from the spherical shape.

    The next step looks like getting the spheres tied to a backplane to pull off the accumulating energy.

    Lay these layers down and seal them in a small air space and you can pull both heat and electricity from a very simple design.  Might even be transparent enough to deposite on window glass.

     

    Cool,

    DAB