Publications
  • Learn
  • More
Publications
Blog Navy Helicopter flown on algae-based fuel
  • Blog
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Publications to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Eavesdropper
  • Date Created: 24 Jun 2011 8:02 PM Date Created
  • Views 685 views
  • Likes 1 like
  • Comments 3 comments
  • alternative_energy
  • defense
  • dit
  • transportation
  • military
  • eavesdropper:dit
  • industry
  • navy
  • energy
  • aerospace
  • innovation
  • biofuel
Related
Recommended

Navy Helicopter flown on algae-based fuel

Eavesdropper
Eavesdropper
24 Jun 2011

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

This first successful flight of a military helicopter using a algae-based biofuel was conducted this week. A MH 60S Seahawk was flown on fuel dubbed Solajet HRJ-5 jet fuel, which is a 50/50 blend of Jet-A and algae-based fuels. The fuel was designed by Honeywell UOP and Solazyme in tandem with the US Navy and DLA-Energy. The concept is to just use the fuel in the vehicle without any modification to the engine. The demonstration went off without a hitch.
 
Solazyme CEO Jonathan Wolfsan said after the test, "We applaud ASTM International and the ATA and CAAFI for their efforts to advance the world’s newest and most sustainable fuels for aviation.  The aviation industry has demonstrated a strong leadership position in fuel supply diversification and sustainability, and today’s announcement is a major step in its efforts to commercialize advanced low-carbon biofuels... and reinforces the Navy’s commitment to securing our nation’s energy supply."
 
A similar 50/50 blend was tested with additional success by the U.S. Air Force on a Globemaster III jet. The military, as a whole, pledges to use 50% renewable energy within ten years. Algae-based fuels are part of the second generation biofuels, and is indeed renewable. Additionally, the U.S. Departement of Energy estimates that to grow enough algae to replace petroleum as a fuel, in the USA, would require an area about 15,000 square miles (39,000 square km). About 0.42% of the US land mass, less than 1/7th of the area used to farm corn. The algae Biomass Organization also claims they can meet price parity with oil by 2018, only if tax credits are awarded. Algae-electric hybrids, anyone?
 
Eavesdropper
  • Sign in to reply
  • DAB
    DAB over 14 years ago in reply to Eavesdropper

    Coal is a whole lot dirtier than oil.  However, I agree, we are wasting a lot of potential fuel by not properly processing our sewage as a resource instead of a waste product.

    I just don't understand why people are so quick to throw things away instead of thinking of new ways to turn it into a positive resource.  Especially due to the quantity of material we are talking about.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Eavesdropper
    Eavesdropper over 14 years ago in reply to DAB

    With the possibility of creating this biofuel from sewage, see here, I think that further harm to the environment is much lower than how oil has ravaged the planet.

     

    E

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 14 years ago

    I am not too surprised that they could use the algae oil mixture.  It is probably about the same as using vegatable oil, which works quite well in this type of engine.  It is definitely a good step, but we need to see if they can generate significant quantities of oil without causing any other issues with the environment.

     

    Thanks,

    DAB

    • Cancel
    • Vote Up 0 Vote Down