Publications
  • Learn
  • More
Publications
Blog New telescope provides early warnings for solar flares, detects distant galaxies and spots space garbage
  • Blog
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Publications to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 11 Dec 2012 7:30 PM Date Created
  • Views 640 views
  • Likes 1 like
  • Comments 2 comments
  • research
  • test
  • space_junk
  • transportation
  • industry
  • hmi
  • telescope
  • space_garbage_man
  • space
  • cabeatwell
  • prototyping
  • measurement
  • space_debris
  • sensor
  • innovation
  • communication
Related
Recommended

New telescope provides early warnings for solar flares, detects distant galaxies and spots space garbage

Catwell
Catwell
11 Dec 2012

image

A small but powerful array. The MWA antenna has sixteen croos dipoles. It is powered by a 35kVA trailer-mounted single phase diesel generator. I'm sure in the expanded form they will have grid connectivity. (via MWA)

 

After five long years of development and construction the Murchison Widefield Array (MWA) Observatory, located in Western Australia, is finally completed and currently undergoing preliminary testing. The array is a joint effort between institutions from the US, India, New Zealand and Australia with a main mission to study the sun, its heliosphere, the Earth’s ionosphere, radio transient phenomena (extremely distant galaxies) and to detect neutral atomic Hydrogen emission from the cosmological ‘Epoch of Reionization’ (AKA: studying the phase-change of hydrogen approx. 400,000 years after the Big Bang). Considered one of the largest radio observatories on the planet, the MWA consists of (currently) 128 (4m X 4m) ‘tiles’ with dual-polarization dipoles that have a frequency spectrum of 80-300MHz which are spread out over an area of almost 2 miles in diameter. Initial testing showed that the observatory could not only observe distant celestial bodies but also those found closer to home. In particular, space junk orbiting in low-earth orbit. Everybody knows that space junk creates an inordinate amount of problems for both astronauts as well as equipment that is deployed in space. Current estimates put the orbiting junk pile at about 21,000 pieces that are 10cm or bigger in size. According to MWA director Steven Tingay, the observatory is capable of continuous tracking of those objects rather than calculating trajectories taken from snapshots. Current tracking methods involve ground-based radar that is capable of following 200 pieces of debris a day while the MWA is theoretically capable of tracking thousands simultaneously, which equates to almost the whole debris field tracked over one night. To test their theory of tracking junk the research team used the MWA to receive FM radio signals bounced off of the ISS, which is over 100m wide, and successfully tracked over a distance of almost 8 miles. While that may not sound so fantastic, the data will be used to refine the radio technique to scale it down to tracking material at 10cm in size. Eventually the Observatory will gain a build-up of 256 tiles in order to gain increased sensitivity and resolution which will make the process that much easier.

 

 

Cabe

http://twitter.com/Cabe_e14

 

See more space debris cleaning options:

Slowing space junk to clean orbiting space, Ballistic Clouds

New satellite aims to chase down and clean up space debris

DARPA looks to implement ‘neighborhood watch’ to gain a handle on space debris

  • Sign in to reply
Parents
  • DAB
    DAB over 13 years ago

    Hi Cabe,

     

    Do you know if they are going to open source their data?

     

    I can think of a number of uses for the data if it comes with good time stamp.

     

    Just a thought,

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 13 years ago

    Hi Cabe,

     

    Do you know if they are going to open source their data?

     

    I can think of a number of uses for the data if it comes with good time stamp.

     

    Just a thought,

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • Catwell
    Catwell over 13 years ago in reply to DAB

    Good question. It appears all the tech and software is proprietary. I am sure they are trying to win some sort of contract.

     

    I will inquire with them and see what their plan is for the future.

     

    If many had a small array, connected together would be quite powerful and useful.

     

    C